etnaviv gpu driver for imx8qxp on rel_imx_4.19.35_1.1.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

etnaviv gpu driver for imx8qxp on rel_imx_4.19.35_1.1.0

1,985 次查看
refiktuzaklı
Contributor III

Hello,

I want to use etnaviv gpu driver for imx8qxp mek.

I disabled MXC_GPU_VIV, enabled DRM_ETNAVIV on arm64 default defconfig.

fls-imx8qxp-mek.dtb also enables gpu core.

As I read after kernel version of 4.18 etnaviv driver enabled for arm64 architecture however after linux booted, "dmesg | grep viv" gives nothing.

Is vivante gpu driver applicable for imx8qxp mek?

Did I miss some point to enable entaviv gpu driver?

Best regards?

标记 (3)
0 项奖励
回复
4 回复数

734 次查看
r_trivedi123
Contributor IV

Hi, Even this issues still persist in kernel v5.15.71 in NXP BSP - kirkstone branch.

We faced it with one of our customer for sway compositor.

[   27.464790] etnaviv-gpu 38000000.gpu: AXI bus error
[   27.469745] etnaviv-gpu 38000000.gpu: MMU fault status 0x00000000
[   27.970450] etnaviv-gpu 38000000.gpu: recover hung GPU!


However we were able to resolve the issue and now its running smooth with the weston and sway compositor with 4GiB RAM usage.

As this was done for the customer we are unable to share the details, in case of support please reach-out to us on rutvij.trivedi@siliconsignals.io or visit www.siliconsignals.io.

--
BR

0 项奖励
回复

844 次查看
ravicalm
Contributor I
@refiktuzaklı how u enabled or disbled the drivers could you please tell me
0 项奖励
回复

1,863 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Refik

etnaviv is community version of gpu driver not supported by nxp,

issue may be posted on meta-fsl-arm mailing list:

meta-freescale@lists.yoctoproject.org | Home 

Offical gpu driver is described in nxp offical documentaion on i.MX Software and Development Tools | NXP 

and can be found in nxp source.codeaurora.org/external/imx/linux-imx  repository
linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,863 次查看
refiktuzaklı
Contributor III

Hello Igor,

NXP 64bit gpu driver does not support opengl sc and Xorg.

Do you have any alternative for for nxp gpu driver?

I guess this drop of properties on gpu drive rises time to market.

Do you have any other plan to eliminate the lack of these properties?

Regards,

0 项奖励
回复