Dear all,
I can not communicate via ethernet with the iMX6 SABRE for Smart Devices. I have been working with some other iMX6 boards before and I am following the same procedure:
In my laptop running ubuntu 14.04 I have a static IP address 192.168.0.50
and the /etc/network/interfaces file in the iMX6 board is:
root@imx6qsabresd:~# cat /etc/network/interfaces
# /etc/network/interfaces -- configuration file for ifup(8), ifdown(8)
# The loopback interface
auto lo
iface lo inet loopback
# Wireless interfaces
#iface wlan0 inet dhcp
# wireless_mode managed
# wireless_essid any
# wpa-driver wext
# wpa-conf /etc/wpa_supplicant.conf
#iface atml0 inet dhcp
# Wired or wireless interfaces
auto eth0
iface eth0 inet static
address 192.168.0.30
netmask 255.255.255.0
gateway 192.168.0.1
#iface eth1 inet dhcp
# Ethernet/RNDIS gadget (g_ether)
# ... or on host side, usbnet and random hwaddr
#iface usb0 inet static
# address 192.168.7.2
# netmask 255.255.255.0
# network 192.168.7.0
# gateway 192.168.7.1
# Bluetooth networking
#iface bnep0 inet dhcp
As you can see, I have disabled everything except for the eth0 configuration, just to be sure there are no additional conflicts.However, after rebooting, the ifconfig config doesn't recognize the eth0 setting in /etc/network/interfaces:
root@imx6qsabresd:~# ifconfig
eth0 Link encap:Ethernet HWaddr 00:04:9F:03:9F:FD
inet addr:169.254.193.228 Bcast:169.254.255.255 Mask:255.255.0.0
inet6 addr: fe80::204:9fff:fe03:9ffd/64 Scope:Link
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:39 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:9835 (9.6 KiB)
lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
inet6 addr: ::1/128 Scope:Host
UP LOOPBACK RUNNING MTU:65536 Metric:1
RX packets:10 errors:0 dropped:0 overruns:0 frame:0
TX packets:10 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:0
RX bytes:700 (700.0 B) TX bytes:700 (700.0 B)
If I do configure it manually, eth0 link is not working properly:
root@imx6qsabresd:~# ifconfig eth0 down
root@imx6qsabresd:~# IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
root@imx6qsabresd:~# ifconfig eth0 192.168.0.30 netmask 255.255.255.0 up
fec 2188000.ethernet eth0: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_addr=2188000.ethernet:01, irq=-1)
root@imx6qsabresd:~# IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
libphy: 2188000.ethernet:01 - Link is Up - 1000/Full
IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
root@imx6qsabresd:~# ifconfig
eth0 Link encap:Ethernet HWaddr 00:04:9F:03:9F:FD
inet addr:192.168.0.30 Bcast:192.168.0.255 Mask:255.255.255.0
inet6 addr: fe80::204:9fff:fe03:9ffd/64 Scope:Link
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:71 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:21095 (20.6 KiB)
lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
inet6 addr: ::1/128 Scope:Host
UP LOOPBACK RUNNING MTU:65536 Metric:1
RX packets:10 errors:0 dropped:0 overruns:0 frame:0
TX packets:10 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:0
RX bytes:700 (700.0 B) TX bytes:700 (700.0 B)
Any suggestion? It is really weird for me (I am not a linux expert at all!)
I don't know what I am missing ....
Thank you very much for your feedback!
Mensaje editado por: Alvaro Martinez
解決済! 解決策の投稿を見る。
For those who may help ... this is what was happening:
There are two network services executing on SABRESD
The one service is Linux network service(/etc/init.d/networking).
The another service is connman (/etc/init.d/connman).
First, static ip was set by Linux network service.
And then, ip address override by connman service.
So, static ip was invalidated by connman.
I'd like to set ip address in simple way.
So, I removed connman service from init.d .
chmod -x /etc/init.d/connman
now it's only reading configuration from /etc/networking/interfaces
For those who may help ... this is what was happening:
There are two network services executing on SABRESD
The one service is Linux network service(/etc/init.d/networking).
The another service is connman (/etc/init.d/connman).
First, static ip was set by Linux network service.
And then, ip address override by connman service.
So, static ip was invalidated by connman.
I'd like to set ip address in simple way.
So, I removed connman service from init.d .
chmod -x /etc/init.d/connman
now it's only reading configuration from /etc/networking/interfaces
Hi Alvaro Martinez
I can't find /etc/init.d/connman
or /etc/init.d/comman
The release of mine is 3.14.52 for sabre-ai
Regards!
Hi yoo Liang.
I also same kernel. 3.14.52 & imx6 sabresd board.
I also not work ethernet to my PC.
Do you solve problem?
Hi,
Have you tried to set the ip from u-boot bootargs?
ip=192.168.0.30 instead of ip=dhcp
/Alejandro
Hi Alejandro,
Thank you for your feedback!
Yes, I had tried it before and it didn't work.
In u-boot I have set ipaddr=192.168.0.30 and netmask=255.255.255.0 and, even serverip=192.168.0.50 (my PC)
Where should I add this ip parameter that you mention?
These are my u-boot parameters:
=> printenv
baudrate=115200
boot_fdt=try
bootcmd=mmc dev ${mmcdev};if mmc rescan; then if run loadbootscript; then run bootscript; else if run loadimage; then run mmcboot; else run netboot; fi; fi; else run netboot; fi
bootcmd_mfg=run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};
bootdelay=2
ootscript=echo Running bootscript from mmc ...; source
console=ttymxc0
ethact=FEC
ethaddr=00:04:9f:03:9f:fd
ethprime=FEC
fdt_addr=0x18000000
fdt_file=imx6q-sabresd.dtb
fdt_high=0xffffffff
image=zImage
initrd_addr=0x12C00000
initrd_high=0xffffffff
ip_dyn=yes
ipaddr=192.168.0.30
loadaddr=0x12000000
loadbootscript=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${script};
loadfdt=fatload mmc ${mmcdev}:${mmcpart} ${fdt_addr} ${fdt_file}
loadimage=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${image}
mfgtool_args=setenv bootargs console=ttymxc0,115200 rdinit=/linuxrc g_mass_storage.stall=0 g_mass_storage.removable=1 g_mass_storage.idVendor=0x066F g_mass_storage.idProduct=0x37FF g_mass_storage.iSerialNumber="" enable_wait_mode=off
mmcargs=setenv bootargs console=${console},${baudrate} ${smp} root=${mmcroot}
mmcautodetect=yes
mmcboot=echo Booting from mmc ...; run mmcargs; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if run loadfdt; then bootz ${loadaddr} - ${fdt_addr}; else if test ${boot_fdt} = try; then bootz; else echo WARN: Cannot load the DT; fi; fi; else bootz; fi;
mmcdev=1
mmcpart=1
mmcroot=/dev/mmcblk2p2 rootwait rw
netargs=setenv bootargs console=${console},${baudrate} ${smp} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp
netboot=echo Booting from net ...; run netargs; if test ${ip_dyn} = yes; then setenv get_cmd dhcp; else setenv get_cmd tftp; fi; ${get_cmd} ${image}; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if ${get_cmd} ${fdt_addr} ${fdt_file}; then bootz ${loadaddr} - ${fdt_addr}; else if test ${boot_fdt} = try; then bootz; else echo WARN: Cannot load the DT; fi; fi; else bootz; fi;
netmask=255.255.255.0
script=boot.scr
serverip=192.168.0.50
update_sd_firmware=if test ${ip_dyn} = yes; then setenv get_cmd dhcp; else setenv get_cmd tftp; fi; if mmc dev ${mmcdev}; then if ${get_cmd} ${update_sd_firmware_filename}; then setexpr fw_sz ${filesize} / 0x200; setexpr fw_sz ${fw_sz} + 1; mmc write ${loadaddr} 0x2 ${fw_sz}; fi; fi
To follow with my explanation, this is what I get immediatly after boot:
root@imx6qsabresd:~# ifconfig
eth0 Link encap:Ethernet HWaddr 00:04:9F:03:9F:FD
inet addr:169.254.193.228 Bcast:169.254.255.255 Mask:255.255.0.0
inet6 addr: fe80::204:9fff:fe03:9ffd/64 Scope:Link
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:39 errors:0 dropped:0 overruns:0 frame:0
TX packets:40 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:2648 (2.5 KiB) TX bytes:9965 (9.7 KiB)
lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
inet6 addr: ::1/128 Scope:Host
UP LOOPBACK RUNNING MTU:65536 Metric:1
RX packets:10 errors:0 dropped:0 overruns:0 frame:0
TX packets:10 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:0
RX bytes:700 (700.0 B) TX bytes:700 (700.0 B)
----------------------------------------------------------------------------------------
but my /etc/network/interfaces is:
root@imx6qsabresd:~# cat /etc/network/interfaces
# /etc/network/interfaces -- configuration file for ifup(8), ifdown(8)
# The loopback interface
auto lo
iface lo inet loopback
# Wireless interfaces
#iface wlan0 inet dhcp
# wireless_mode managed
# wireless_essid any
# wpa-driver wext
# wpa-conf /etc/wpa_supplicant.conf
#iface atml0 inet dhcp
# Wired or wireless interfaces
auto eth0
iface eth0 inet static
address 192.168.0.30
netmask 255.255.255.0
gateway 192.168.0.1
#iface eth1 inet dhcp
# Ethernet/RNDIS gadget (g_ether)
# ... or on host side, usbnet and random hwaddr
#iface usb0 inet static
# address 192.168.7.2
# netmask 255.255.255.0
# network 192.168.7.0
# gateway 192.168.7.1
# Bluetooth networking
#iface bnep0 inet dhcp
-----------------------------------------------------------------------------------------------
if then, I execute /etc/init.d/networking restart, then it works!
root@imx6qsabresd:~# /etc/init.d/networking restart
Running /etc/init.d/networking restart is deprecated because it may not enable again some interfaces
Reconfiguring network interfaces...
fec 2188000.ethernet eth0: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_addr=2188000.ethernet:01, irq=-1)
done.
root@imx6qsabresd:~# IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
libphy: 2188000.ethernet:01 - Link is Up - 1000/Full
IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
root@imx6qsabresd:~# ifconfig
eth0 Link encap:Ethernet HWaddr 00:04:9F:03:9F:FD
inet addr:192.168.0.30 Bcast:192.168.0.255 Mask:255.255.255.0
inet6 addr: fe80::204:9fff:fe03:9ffd/64 Scope:Link
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:156 errors:0 dropped:0 overruns:0 frame:0
TX packets:76 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:11200 (10.9 KiB) TX bytes:21125 (20.6 KiB)
lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
inet6 addr: ::1/128 Scope:Host
UP LOOPBACK RUNNING MTU:65536 Metric:1
RX packets:10 errors:0 dropped:0 overruns:0 frame:0
TX packets:10 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:0
RX bytes:700 (700.0 B) TX bytes:700 (700.0 B)
Any idea?
Thank you for your time and help!
alvaro
Hi,
If you want the script interfaces to take effect I would try with
>ifdown eth0
>ifup eth0
An "ifconfig up eth0" activates eth0 but does not setup IP addresses.
Best Regards,
Alejandro
Thank you for your answer!
If after boot process, I execute what you have suggested or /etc/init.d/networking restart
it works ....
What could I do not to be forced to do it each time I power up the sabresd?
Regards,
alvaro