end Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(179,98)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

end Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(179,98)

1,427 Views
shahin22
Contributor I

I have built the image for IMX8M Plus using Yocto and put it on SD card. While booting hardware through SD card I am getting error "[ 3.793856] ---[ end Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(179,98) ]---"

I have attached the log file here.

0 Kudos
Reply
4 Replies

1,363 Views
shahin22
Contributor I

Hardware name: NXP i.MX8MPlus EVK board (DT)

urn the immage on sd card using this step-/yocto/imx-yocto-bsp/build-xwayland/tmp/deploy/images/imx8mp-lpddr4-evk$ zstdcat imx-image-full-imx8mp-lpddr4-evk-20230825110715.rootfs.wic.zst | sudo dd of=/dev/sdb bs=1M conv=fsync

 

0 Kudos
Reply

1,341 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @shahin22!

Please follow the steps of the chapter "4.2 Universal update utility" or chapter "4.3 Preparing an SD/MMC card to boot" in our Linux user guide, those chapters describe how to deploy the system using the uuu or with Linux commands.

https://www.nxp.com/docs/en/user-guide/IMX_LINUX_USERS_GUIDE.pdf

If the problem persists, I recommend checking using our precompiled images if you made a modification in the Yocto Project.

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...


Best Regards!

Chavira

0 Kudos
Reply

784 Views
awarakhan
Contributor I

Were you able to solve this issue, i have same.

0 Kudos
Reply

1,396 Views
Chavira
NXP TechSupport
NXP TechSupport

Thank you for contacting NXP Support!

What board are you using?

What steps are you using to write the SD card?

I recommend using the UUU to deploy the system on your board.

Best Regards!

Chavira

0 Kudos
Reply