eglSwapBuffers suddenly slows down!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

eglSwapBuffers suddenly slows down!

ソリューションへジャンプ
1,157件の閲覧回数
Takashi_Kashiwagi
Senior Contributor I

Hi Community.

 

I'm using IMX8MM with yocto linux 4.19.

We are investigating why our Qt application has a low FPS.

And I found that "eglSwapBuffers" suddenly slowed down as follows.

samplingaverage[ms]min[ms]max[ms]STDEV.P
100000.6510.1671661.19720.79986144

 

I don't know the cause so far, but is there any workaround?

 

Best Regards,

T.Kashiwagi

ラベル(3)
0 件の賞賛
返信
1 解決策
1,149件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Takashi san,

If eglSwapbuffers is writting bytes on the next memory page this should be a bug in the vivante driver, rendering activity for one frame has very clearly defined demarcation of what is one frame and what is the next.

However in case of your issue, this is not reproducible in the Yocto BSP that NXP provides, Please provide a sample code to reproduce in our side and get the fix from the developers team, GPU drivers are propietary and are just provided in binary form.

 

Regards

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,150件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Takashi san,

If eglSwapbuffers is writting bytes on the next memory page this should be a bug in the vivante driver, rendering activity for one frame has very clearly defined demarcation of what is one frame and what is the next.

However in case of your issue, this is not reproducible in the Yocto BSP that NXP provides, Please provide a sample code to reproduce in our side and get the fix from the developers team, GPU drivers are propietary and are just provided in binary form.

 

Regards

0 件の賞賛
返信
1,143件の閲覧回数
Takashi_Kashiwagi
Senior Contributor I

Hi Bio-san

 

Thank you for reply!

 

However in case of your issue, this is not reproducible in the Yocto BSP that NXP provides, Please provide a sample code to reproduce in our side and get the fix from the developers team, GPU drivers are propietary and are just provided in binary form.

OK. I wil discuss within my team.

 

Best Regards,

T.Kashiwagi

0 件の賞賛
返信