eclipse, arm-poky-linux-gnueabi/4.9.2/ld: cannot find crti.o

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

eclipse, arm-poky-linux-gnueabi/4.9.2/ld: cannot find crti.o

2,226 Views
olias
Contributor II

Hello,

I built a simple hello_world.c test program on the command line:

arm-poky-linux-gnueabi-gcc test1.c -v -march=armv7-a -mfloat-abi=hard -mfpu=neon -mtune=cortex-a9

--sysroot=/opt/fsl-imx-fb/3.14.52-1.1.1/sysroots/cortexa9hf-vfp-neon-poky-linux-gnueabi/

-I /opt/fsl-imx-fb/3.14.52-1.1.1/sysroots/cortexa9hf-vfp-neon-poky-linux-gnueabi/usr/include/ -o hello

Works fine.

I setup Eclipse IDE for a c project and set all the env variables, and so forth as one would expect.

I tried all sorts of tricks but I get:

Invoking: Cross GCC Linker

arm-poky-linux-gnueabi-gcc -L/opt/fsl-imx-fb/3.14.52-1.1.1/sysroots/cortexa9hf-vfp-neon-poky-linux-gnueabi/lib

-L/opt/fsl-imx-fb/3.14.52-1.1.1/sysroots/cortexa9hf-vfp-neon-poky-linux-gnueabi/usr/lib -o "hello"  ./src/hello.o

 

/opt/fsl-imx-fb/3.14.52-1.1.1/sysroots/x86_64-pokysdk-linux/usr/libexec/arm-poky-linux-gnueabi/gcc/arm-poky-linux-gnueabi/4.9.2/ld: cannot find crt1.o: No such file or directory

makefile:30: recipe for target 'test1' failed

/opt/fsl-imx-fb/3.14.52-1.1.1/sysroots/x86_64-pokysdk-linux/usr/libexec/arm-poky-linux-gnueabi/gcc/arm-poky-linux-gnueabi/4.9.2/ld: cannot find crti.o: No such file or directory

/opt/fsl-imx-fb/3.14.52-1.1.1/sysroots/x86_64-pokysdk-linux/usr/libexec/arm-poky-linux-gnueabi/gcc/arm-poky-linux-gnueabi/4.9.2/ld: cannot find crtbegin.o: No such file or directory

collect2: error: ld returned 1 exit status

make: *** [test1] Error 1

The  -L/opt/fsl-imx-fb/3.14.52-1.1.1/sysroots/cortexa9hf-vfp-neon-poky-linux-gnueabi/usr/lib is where these files are.

The command line works fine when I export the env vars before hand.

This is a Yocto toolchain SDK built for the QWKS-SCMIMX6DQ installed in /opt which built a working image.

Any clues?

Labels (3)
Tags (1)
0 Kudos
1 Reply

701 Views
jimmychan
NXP TechSupport
NXP TechSupport