eMMC pSLC mode support for i.MX25

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

eMMC pSLC mode support for i.MX25

跳至解决方案
1,259 次查看
yuuki
Senior Contributor II

Dear all,

We want to use eMMC memory with pSLC mode with i.MX25.

In this case, it is necessary for [156]PARTITIONS_ATTRIBUTE of Extended CSD Register to be programed

However, the eMMC I/F of i.MX25 is Specification Version 4.2.

We understand that Version 4.2 does not support this operation.

Can eMMC of i.MX25 support pSLC mode by software modification?

(Can [156]PARTITIONS_ATTRIBUTE of Extended CSD Register be programed by software?)

May I have advice?

Best Regards,
Yuuki

标签 (1)
0 项奖励
回复
1 解答
694 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

>(Can [156]PARTITIONS_ATTRIBUTE of Extended CSD Register be programed by software?)

yes, i.MX25 SDHC support such operation using CMD6 and this is described in

Table 23-30. Commands for MMC/SD/SDIO/CE-ATA Cards i.MX25 Reference Manual (rev.2, 1/2011)

http://www.freescale.com/files/dsp/doc/ref_manual/IMX25RM.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
695 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

>(Can [156]PARTITIONS_ATTRIBUTE of Extended CSD Register be programed by software?)

yes, i.MX25 SDHC support such operation using CMD6 and this is described in

Table 23-30. Commands for MMC/SD/SDIO/CE-ATA Cards i.MX25 Reference Manual (rev.2, 1/2011)

http://www.freescale.com/files/dsp/doc/ref_manual/IMX25RM.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复