eMMC burning with MFG Tool

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

eMMC burning with MFG Tool

1,496 次查看
mach_lee
Contributor II

Hi,

My board is MX6Q with eMMC boot configured and NOT EVM available in the market.

I have some problem of burning eMMC with MFG Tool (L4.1.15_2.0.0-ga_mfg-tools)

If I save the cfg.ini like below...

[profiles]
chip = Linux

[platform]
board = SabreSD

[LIST]
name = eMMC

[variable]
board =
plus

then the MfgTool.log is

DLL version: 2.7.0
Wednesday, June 21, 2017 19:52:31 Start new logging
ModuleID[2] LevelID[1]: Boot command-- file I:\Freescale\MFG_TOOL\L4.1.15_2.0.0-ga_mfg-tools\mfgtools-with-rootfs\mfgtools\Profiles\Linux\OS Firmware\firmware\u-boot-imx6q.imx failed to open.errcode is 2
ModuleID[2] LevelID[1]: Parse ucl script failed, error code: 4

But I try like below.....

[profiles]
chip = Linux

[platform]
board = SabreSD

[LIST]
name = eMMC

[variable]
board = einsys
plus =

then the log is 

DLL version: 2.7.0
Wednesday, June 21, 2017 19:55:16 Start new logging
ModuleID[2] LevelID[1]: Boot command-- file I:\Freescale\MFG_TOOL\L4.1.15_2.0.0-ga_mfg-tools\mfgtools-with-rootfs\mfgtools\Profiles\Linux\OS Firmware\firmware\u-boot-imx6dleinsys_sd.imx failed to open.errcode is 2
ModuleID[2] LevelID[1]: Parse ucl script failed, error code: 4

My question is how MFG tool read the CPU code in wrong.

Can anyone help me, please...?

The ucl2.xml modified part is this

<CMD state="BootStrap" type="boot" body="BootStrap" file ="firmware/u-boot-imx6q%plus%%board%.imx" ifdev="MX6Q">Loading U-boot</CMD>

from

<CMD state="BootStrap" type="boot" body="BootStrap" file ="firmware/u-boot-imx6q%plus%%board%_sd.imx" ifdev="MX6Q">Loading U-boot</CMD>

标签 (1)
0 项奖励
1 回复

590 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Mach

seems mfg tool can not find these files in folder, as replacing %board% with einsys

it will look for u-boot-imx6q%plus%einsys.imx file. In general it is not necessary to modify

cfg.ini file, just click on *.vbs file and mfg tool will start with parameters provided by *.vbs file.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励