Hi
booting from a eMMC 4.5 device is not supported, boot ROM will fall back to the
eMMC4.4 standard when a eMMC4.5 capable device is detected.
In BSP it is possible to bypass eMMC version checking, so that eMMC v4.5 can
work as eMMC v4.4 cards, no specific v4.5 feature supported.
Only basic read/write operations are supported.
static int mmc_read_ext_csd(struct mmc_card *card, u8 *ext_csd)
}
card->ext_csd.rev = ext_csd[EXT_CSD_REV];
- if (card->ext_csd.rev > 5) {
+ /* workaround: support emmc 4.5 cards to work at emmc 4.4 mode */
+ if (card->ext_csd.rev > 6)
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi
booting from a eMMC 4.5 device is not supported, boot ROM will fall back to the
eMMC4.4 standard when a eMMC4.5 capable device is detected.
In BSP it is possible to bypass eMMC version checking, so that eMMC v4.5 can
work as eMMC v4.4 cards, no specific v4.5 feature supported.
Only basic read/write operations are supported.
static int mmc_read_ext_csd(struct mmc_card *card, u8 *ext_csd)
}
card->ext_csd.rev = ext_csd[EXT_CSD_REV];
- if (card->ext_csd.rev > 5) {
+ /* workaround: support emmc 4.5 cards to work at emmc 4.4 mode */
+ if (card->ext_csd.rev > 6)
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------