drivers for serializer(DS90UB927Q-Q1)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

drivers for serializer(DS90UB927Q-Q1)

797件の閲覧回数
rambabugedela
Contributor I

hi,

I am working on serializer (DS90UB927Q-Q1) for sabresd board (IMX6dl) but I found that there no drivers for DS90UB927Q-Q1. Anybody help me plz.

ラベル(4)
0 件の賞賛
返信
1 返信

510件の閲覧回数
art
NXP Employee
NXP Employee

Do you use the i.MX6 series Linux BSP by NXP? If so, to perform the serializer IC configuration through the I2C control interface, you can use the low-level I2C driver, already included into the system. For more details, refer to the Chapter 37 of the attached document. In all other aspects, no other special driver is required for the DS90UB927Q serializer IC operation.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信