does imx6 yocto5.4.70 support wayland ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

does imx6 yocto5.4.70 support wayland ?

904 Views
jiangyaqiang
Contributor V

HI anyone:

 

  Does imx6 yocto5.4.70 support wayland ?

  I have follow the user guild of yocto in "imx-yocto-L5.4.70_2.3",  and I found that, it will fail to bitbake imx-image-full for imx6q/dl when using DISTRO=fsl-imx-xwayland or  DISTRO=fsl-imx-wayland. it's no problem to bitbake imx-image-multimedia.

   It said missing "drm", but the "drm" source is downloaded.


  Could anyone give me a hand ?

  here is the fail log:

ERROR: qtwayland-5.15.0+gitAUTOINC+0f847b7688-r0 do_configure: Error calling /home/hms/harddisk_3t_1/hansen/ibr215-yocto-bitbake2/ibr117-waylan2/tmp/work/cortexa9t2hf-neon-mx6qdl-poky-linux-gnueabi/qtwayland/5.15.0+gitAUTOINC+0f847b7688-r0/recipe-sysroot-native/usr/bin/qmake -makefile -o Makefile QT_BUILD_PARTS-=examples QT_BUILD_PARTS-=tests /home/hms/harddisk_3t_1/hansen/ibr215-yocto-bitbake2/ibr117-waylan2/tmp/work/cortexa9t2hf-neon-mx6qdl-poky-linux-gnueabi/qtwayland/5.15.0+gitAUTOINC+0f847b7688-r0/git/qtwayland.pro -- -no-feature-wayland-brcm -feature-wayland-client -no-feature-wayland-drm-egl-server-buffer -feature-wayland-egl -no-feature-wayland-libhybris-egl-server-buffer -feature-wayland-server -no-feature-xcomposite-egl -no-feature-xcomposite-glx
ERROR: qtwayland-5.15.0+gitAUTOINC+0f847b7688-r0 do_configure: Execution of '/home/hms/harddisk_3t_1/hansen/ibr215-yocto-bitbake2/ibr117-waylan2/tmp/work/cortexa9t2hf-neon-mx6qdl-poky-linux-gnueabi/qtwayland/5.15.0+gitAUTOINC+0f847b7688-r0/temp/run.do_configure.5916' failed with exit code 1:

Running configuration tests...
Project ERROR: Test config.qtwayland_client.tests.dmabuf-server-buffer tries to use undeclared library 'drm'
WARNING: exit code 1 from a shell command.

ERROR: Logfile of failure stored in: /home/hms/harddisk_3t_1/hansen/ibr215-yocto-bitbake2/ibr117-waylan2/tmp/work/cortexa9t2hf-neon-mx6qdl-poky-linux-gnueabi/qtwayland/5.15.0+gitAUTOINC+0f847b7688-r0/temp/log.do_configure.5916

 

 

Labels (2)
Tags (1)
0 Kudos
Reply
2 Replies

896 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Supported, Setup for Wayland:
$: DISTRO=fsl-imx-wayland MACHINE=<machine name> source imx-setup-release.sh -b build-wayland

0 Kudos
Reply

893 Views
jiangyaqiang
Contributor V

HI :

   Thanks, I have do that,it's ok for bitbake fsl-image-mutilmedia.

   But fail in bitbake fsl-image-full, it shows the log as I provided before.

   I have also try DISTRO=fsl-imx-xwayland MACHINE=<machine name> source imx-setup-release.sh -b build-wayland, it fail too.

0 Kudos
Reply