differences in industrial, Automotive and consumer i.mx6 quad applications application processors

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

differences in industrial, Automotive and consumer i.mx6 quad applications application processors

1,053件の閲覧回数
famavela
Contributor I

Dear i.MX Developers,

I need to know about i.mx6 quad differences in industrial, Automotive and consumer applications. Can I use android OS that is developed for i.mx6 quad consumer application processor with i.mx6 quad industrial application processor.

Best Regards.

ラベル(3)
0 件の賞賛
返信
2 返答(返信)

764件の閲覧回数
Yuri
NXP Employee
NXP Employee

Please refer to the following resource regarding Freescale Product Qualification.

http://www.freescale.com/webapp/sps/site/overview.jsp?code=QUALITY__QUALIF

As for i.MX6 – using i.mx6 quad industrial device instead of consumer one – generally,

yes it is possible, but when selecting i.MX6 part numbers, please pay attention on

VPU, GPU, MLB modules presence and CPU frequency ratings, using corresponding hardware

specs in the Datasheets. Please refer to Figure 1 (Part Number Nomenclature -i.MX 6Quad

and i.MX 6Dual).

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQIEC.pdf

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

764件の閲覧回数
famavela
Contributor I

hi

thank you for quick response.

i just want to specify my question.

my question exactly is, "i.MX6 Quad consumer processor can be used in industrial tablets? because of having high performance of consumer version beside harsh environments endurance".

more detail, i want ask "extra heat sinks can help consumer processors to act like industrial/automotive versions"?

generally what is freescale suggestion for  high performance industrial tablets ?

0 件の賞賛
返信