could u please share me mx6q sabresd board .sd card image.
in this download only contain imx6soloboard image
please reply its urgent one
Hai yuri ,
I created sdb1 partition on Sd card. because at the starting sd card have no partition .
then i copied that solo image to sd card. but it is not working the imx6Qsabresd evaluation kit.
please reply me.
it's urgent one
Have You used the Linux host to deploy the image with the following command ?
$ sudo dd if= fsl-image-qt5-x11-imx6qdlsolo.sdcard of=/dev/sdb1 bs=1M
After that insert the SD card to the board and power on ?
Are Your boot configuration correct ? Please check it - SD3 boot.
Regards,
Yuri.
Hi Yuri,
I did some test and tried if I can post on community.
Please ignore or reject my content.
Annie
could u please share me the working "fsl-image-gui-x11-imx6qdlsolo.sdcard
Hai yuri ,
Thanks for the response
I have one doubt when i mount my SD card
i listed out drivers in ls /dev
i can find only sdb
sdb is my SD card
there is no sdb1 when i am copying this image by using this command sudo dd if= fsl-image-qt5-x11-imx6qdlsolo.sdcard of=/dev/sdb1 bs=1M
through this command sdb1 partition created in disk or device ?
hai yuri its working...
thanks..
let me know in this demo image contain any qt application . ?
could u please tell me the location of the qt application?
please tell meee
Hai Yuri ,
I copied the image by using this command sudo dd if= fsl-image-qt5-x11-imx6qdlsolo.sdcard of=/dev/sdb1 bs=1M
after that the SD card is put in board. i didnt passs any boot arguemts the boot loader log is also not shown in teraterm
my Evaluation kit is MCIMX6Q-SDP
please help me
its an urgent issue
hai yuri ,
I copied the image by using sudo dd if= fsl-image-qt5-x11-imx6qdlsolo.sdcard of=/dev/sdb1 bs=1M this command.
but it is not loading ,uboot also not loading ...
please help me
let me know u tried out in MX6Qsabresd board
my board is working.
Now i download android prebuilt image by using MFG tool. this is working properly in my board
could u please help me to flash the image by using mfg tool give me the mfgtool image ,mfgtool for downloading the prebuilt image to my board
Hai Ruihong ,
I have tested with these two images in mx6qsabresd evaluation kit which purchased from freescale ( fsl-image-qt5-x11-imx6qdlsolo.sdcard ,fsl-image-gui-x11-imx6qdlsolo.sdcard) both the images are not booting imx6qsabresd board evaluation kit.
could u please help me to solve this issue
could u please give me the exact image for imx6qsabrsd board