I'm compiling linux image (4.14) for an i.mx6QP and noticed that cpufreq doesn't show up under /sys/devices/systems/cpu/cpu0
What could the be reason why it doesn't show up?
解決済! 解決策の投稿を見る。
Found the issue.
There was mistake in my .dts file.
Hi Niklas
please try L4.1.15 offical nxp bsps (there is no 4.14) described on
i.MX 6 / i.MX 7 Series Software and Development Tool|NXP
cpufreq driver is described in Chapter 23 CPU Frequency Scaling (CPUFREQ) Driver
attached Linux Manual.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor.
Thanks for your response.
The reason we we decided to go for the latest Linux version because we could not get the PCI to work in our design when using 4.1.x version.
I know the CPU frequency driver worked when we were running the image on an i.mx6D, but when I ran on the i.mxQP it didn't show up.
The only difference is that I had to change u-boot when running on the QP version.
Regards,
Niklas
Hi Niklas
there are several kernels and versions but not all of them have comprehensive
i.MX6QP support
[meta-freescale] Issue with freescale git server at git.freescale.com
suggest to test with nxp official bsps described on
i.MX 6 / i.MX 7 Series Software and Development Tool|NXP
Best regards
igor
Hi Igor.
For the moment I'm just interested to see that it's running with full speed.
Is there an easy way to verify that it's running with the highest frequency (since I don't have access the frequency info kernel). Or is it to just read some of the registers to see what the clock is set to?
Regards,
Niklas
Hi Niklas
one can output arm_clk_root on CLKO pin using CCM_CCOSR register
and test it with oscilloscope.
Best regards
igor