----------------------------------------------------------------------------
linux@ubuntu:~/fsl-release-bsp/build_x11_imx6ulevk$ bitbake -c cleanall cpuburn-neon
...
linux@ubuntu:~/fsl-release-bsp/build_x11_imx6ulevk$ bitbake cpuburn-neon
WARNING: Host distribution "ubuntu-14.04" has not been validated with this version of the build system; you may possibly experience unexpected failures. It is recommended that you use a tested distribution.
Loading cache: 100% |######################################################################################################################################| Time: 0:00:01
Loaded 3262 entries from dependency cache.
Parsing recipes: 100% |####################################################################################################################################| Time: 0:00:01
Parsing of 2423 .bb files complete (2421 cached, 2 parsed). 3264 targets, 218 skipped, 8 masked, 0 errors.
NOTE: Resolving any missing task queue dependencies
Build Configuration:
BB_VERSION = "1.36.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "ubuntu-14.04"
TARGET_SYS = "arm-poky-linux-gnueabi"
MACHINE = "imx6ulevk"
DISTRO = "fsl-imx-x11"
DISTRO_VERSION = "4.9.88-2.0.0"
TUNE_FEATURES = "arm armv7ve vfp neon callconvention-hard cortexa7"
TARGET_FPU = "hard"
meta
meta-poky = "HEAD:0ec241873367e18f5371a3ad9aca1e2801dcd4ee"
meta-oe
meta-multimedia = "HEAD:dacfa2b1920e285531bec55cd2f08743390aaf57"
meta-freescale = "HEAD:49ac225a38f6d84519798e3264f2e4d19b84f70a"
meta-freescale-3rdparty = "HEAD:1d6d5961dbf82624b28bb318b4950a64abc31d12"
meta-freescale-distro = "HEAD:0ec6d7e206705702b5b534611754de0787f92b72"
meta-bsp
meta-sdk = "HEAD:d65692ecb3a4136fc1cc137152634e8633ddb3c6"
meta-browser = "HEAD:d6f9aed41c73b75a97d71bff060b03a66ee087b1"
meta-gnome
meta-networking
meta-python
meta-filesystems = "HEAD:dacfa2b1920e285531bec55cd2f08743390aaf57"
meta-qt5 = "HEAD:32bb7d18a08d1c48873d7ab6332d4cc3815a4dff"
Initialising tasks: 100% |#################################################################################################################################| Time: 0:00:00
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
WARNING: cpuburn-neon-20140626-r0 do_fetch: Failed to fetch URL https://raw.githubusercontent.com/ssvb/cpuburn-arm/dd5c5ba58d2b0b23cfab4a286f9d3f5510000f20/cpuburn-..., attempting MIRRORS if available
ERROR: cpuburn-neon-20140626-r0 do_fetch: Fetcher failure: Fetch command export DBUS_SESSION_BUS_ADDRESS="unix:abstract=/tmp/dbus-8tsh3O4PKj"; export SSH_AUTH_SOCK="/run/user/1000/keyring-7sbbdb/ssh"; export PATH="/home/linux/fsl-release-bsp/sources/poky/scripts:/home/linux/fsl-release-bsp/build_x11_imx6ulevk/tmp/work/cortexa7hf-neon-poky-linux-gnueabi/cpuburn-neon/20140626-r0/recipe-sysroot-native/usr/bin/arm-poky-linux-gnueabi:/home/linux/fsl-release-bsp/build_x11_imx6ulevk/tmp/work/cortexa7hf-neon-poky-linux-gnueabi/cpuburn-neon/20140626-r0/recipe-sysroot/usr/bin/crossscripts:/home/linux/fsl-release-bsp/build_x11_imx6ulevk/tmp/work/cortexa7hf-neon-poky-linux-gnueabi/cpuburn-neon/20140626-r0/recipe-sysroot-native/usr/sbin:/home/linux/fsl-release-bsp/build_x11_imx6ulevk/tmp/work/cortexa7hf-neon-poky-linux-gnueabi/cpuburn-neon/20140626-r0/recipe-sysroot-native/usr/bin:/home/linux/fsl-release-bsp/build_x11_imx6ulevk/tmp/work/cortexa7hf-neon-poky-linux-gnueabi/cpuburn-neon/20140626-r0/recipe-sysroot-native/sbin:/home/linux/fsl-release-bsp/build_x11_imx6ulevk/tmp/work/cortexa7hf-neon-poky-linux-gnueabi/cpuburn-neon/20140626-r0/recipe-sysroot-native/bin:/home/linux/fsl-release-bsp/sources/poky/bitbake/bin:/home/linux/fsl-release-bsp/build_x11_imx6ulevk/tmp/hosttools"; export HOME="/home/linux"; /usr/bin/env wget -t 2 -T 30 -nv --passive-ftp --no-check-certificate -P /home/linux/fsl-release-bsp/downloads//cpuburn-neon-20140626 'https://raw.githubusercontent.com/ssvb/cpuburn-arm/dd5c5ba58d2b0b23cfab4a286f9d3f5510000f20/cpuburn-a8.S' --progress=dot -v failed with exit code 4, output:
--2020-07-14 14:03:14-- https://raw.githubusercontent.com/ssvb/cpuburn-arm/dd5c5ba58d2b0b23cfab4a286f9d3f5510000f20/cpuburn-...
Resolving raw.githubusercontent.com (raw.githubusercontent.com)... 0.0.0.0, ::
Connecting to raw.githubusercontent.com (raw.githubusercontent.com)|0.0.0.0|:443... failed: Connection refused.
Connecting to raw.githubusercontent.com (raw.githubusercontent.com)|::|:443... failed: Connection refused.
ERROR: cpuburn-neon-20140626-r0 do_fetch: Fetcher failure for URL: 'https://raw.githubusercontent.com/ssvb/cpuburn-arm/dd5c5ba58d2b0b23cfab4a286f9d3f5510000f20/cpuburn-a8.S;name=ssvb'. Unable to fetch URL from any source.
ERROR: cpuburn-neon-20140626-r0 do_fetch: Function failed: base_do_fetch
ERROR: Logfile of failure stored in: /home/linux/fsl-release-bsp/build_x11_imx6ulevk/tmp/work/cortexa7hf-neon-poky-linux-gnueabi/cpuburn-neon/20140626-r0/temp/log.do_fetch.3793
ERROR: Task (/home/linux/fsl-release-bsp/sources/meta-openembedded/meta-oe/recipes-benchmark/cpuburn/cpuburn-neon_20140626.bb:do_fetch) failed with exit code '1'
NOTE: Tasks Summary: Attempted 449 tasks of which 448 didn't need to be rerun and 1 failed.
Summary: 1 task failed:
/home/linux/fsl-release-bsp/sources/meta-openembedded/meta-oe/recipes-benchmark/cpuburn/cpuburn-neon_20140626.bb:do_fetch
Summary: There were 2 WARNING messages shown.
Summary: There were 3 ERROR messages shown, returning a non-zero exit code.
----------------------------------------------------------------------------
Thank you! My network here cannot download cpuburn-neon-20140626 . I copied it from a friend and it has been compiled successfully . Although, please provide a official cpuburn-neon version, only cpuburn-neon cannot be downloaded @ L4.9.88_2.0.0
Yes, it will OK you get the package and copy to you directory and then compile. I do not have the L4.9.88_2.0.0 version source code in my PC, I will ask my colleagues if they have and then share to you.