connet imx6q csi0 to the 10 bit camera interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

connet imx6q csi0 to the 10 bit camera interface

537件の閲覧回数
heziganghe
Contributor I

Hello, I would like to consult a problem that how imx6q connect to the 10 bit camera interface, use  csi0  of  imx6q Interface?thanks!

ラベル(1)
タグ(1)
0 件の賞賛
1 返信

437件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi hezigang

for camera parallel interface connection one can look at

Sabre schematic SPF-27392 p.8, OV5642

SABRE for Smart Devices Reference Design|Freescale

and sect.4.11.10.1 IPU Sensor Interface Signal Mapping

i.MX6DQ Datasheet (rev.4, 7/2015)

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛