Hi All
I have a usb camera that gave raw video as 'YUYV'. I want to use this raw video and encode with imxvpuenc_h264. sadly the imxvpuenc_h264 support I420 as input(SINK) format. which hardware plugin could i be used for conversion from YUYV to I420. The imxipuvideotransform module have Source pad capability of I420 but no Sink pad capability of YUYV.
Hi Artur
Thank you for the quick reply.
As per the document i couldn't find the plugin "imxvideoconvert_ipu" . In my setup i have "imxipuvideotransform" . My imxipu plugin version is 0.11.1. I think these are the same modules but have different version. could you please post the source pad and sink pad capabilities of the module imxvideoconvert_ipu. If the imxvideoconvert_ipu have SINK pad capability of YUYV (YUY2, Not UYVY) then i could update the imxipu plugin.
Thank you
Refer to the Chapter 7 "Multimedia", especially, to the Section 7.3.14 "Video conversion" of the attached document. Use the 'gst-inspect-1.0 imxvideoconvert_ipu' command for the features list.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------