cmake error: yocto(dora) + meta-qt5(dizzy) on imx6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

cmake error: yocto(dora) + meta-qt5(dizzy) on imx6

771 Views
luiscamacho
Contributor I

Hello,

I'm trying to build an image for the SabreLite board, I cloned yocto-dora and meta-qt5 (dizzy).  At compile (bitbake), I'm getting the following error: ..../cmake-native_2.8.11.2.bb, do_configure) failed with exit code '1'

So far, I gathered that the file Qt5CoreConfigExtras.cmake may not have the right path for the qt5 binaries.  So, I input:

..../fsl-community-bsp/build/tmp/sysroots/x86_64-linux/usr/bin/qt5

It still produces the same error.  Can anyone please advise on how to fix this cmake error?

Thank you!

Labels (2)
0 Kudos
Reply
0 Replies