chain of trust HAB imx6UL - encrypted kernel

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

chain of trust HAB imx6UL - encrypted kernel

616 Views
giuliodominutti
Contributor III

References were really helpful in encryption and decryption of a key, following them now under linux I'm able to generate a key blob that is used for encryption of the file system.

But I'm still lost on my second question. There is a way to decrypt an encrypted-kernel? because at the moment I can encrypt u-boot and final file system, but not the images in the middle (boot-script,device tree and kernel). Do you have something useful also for this problem? Thank you

0 Kudos
1 Reply

479 Views
Yuri
NXP Employee
NXP Employee

Hello,

   Sorry, but the information you are requesting is treated as confidential info at this time and requires a signed NDA

(Non-Disclosure Agreement). Naturally, we cannot discuss this with you in public anyway, this requires to be handled

as a Service Request (SR).  If you have not signed an agreement, please contact our distributors.

Distributor Network|NXP 

Have a great day,
Yuri

-------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-------------------------------------------------------------------------------

0 Kudos