Hello!
I build toolchain for iMX6 from GitHub - Freescale/fsl-community-bsp-platform: BSP platform manifest
Follow my steps:
- mkdir /yocto && cd /yocto
- repo init -u https://github.com/Freescale/fsl-community-bsp-platform -b jethro && repo sync
- ./setup-environment /yocto/build
- cd /yocto/build
- bitbake meta-toolchain
- cd tmp/deploy/sdk && ./poky-glibc-x86_64-meta-toolchain-cortexa9hf-vfp-neon-toolchain-2.0.1.sh -y
Tollchain install in /opt/poky/2.0.1, after this I export variables from /opt/poky/2.0.1/environment-setup-cortexa9hf-vfp-neon-poky-linux-gnueabi, file attached.
Now I try compile iperf3:
- cd iperf3
- CC=$(CROSS_COMPILE)gcc ./configure --prefix=/usr --host=arm-poky-linux-gnueabi
Unfortunately configuration failed, follow part configure.log file:
configure:3253: arm-poky-linux-gnueabi-gcc -qversion >&5
arm-poky-linux-gnueabi-gcc: error: unrecognized command line option '-qversion'
arm-poky-linux-gnueabi-gcc: fatal error: no input files
compilation terminated.
configure:3264: $? = 1
configure:3284: checking whether the C compiler works
configure:3306: arm-poky-linux-gnueabi-gcc -O2 -pipe -g -feliminate-unused-debu
g-types -Wl,-O1 -Wl,--hash-style=gnu -Wl,--as-needed conftest.c >&5
/opt/poky/2.0.1/sysroots/x86_64-pokysdk-linux/usr/libexec/arm-poky-linux-gnueabi
/gcc/arm-poky-linux-gnueabi/5.2.0/real-ld: cannot find crt1.o: No such file or d
irectory
/opt/poky/2.0.1/sysroots/x86_64-pokysdk-linux/usr/libexec/arm-poky-linux-gnueabi
/gcc/arm-poky-linux-gnueabi/5.2.0/real-ld: cannot find crti.o: No such file or d
irectory
/opt/poky/2.0.1/sysroots/x86_64-pokysdk-linux/usr/libexec/arm-poky-linux-gnueabi
/gcc/arm-poky-linux-gnueabi/5.2.0/real-ld: cannot find crtbegin.o: No such file
or directory
/opt/poky/2.0.1/sysroots/x86_64-pokysdk-linux/usr/libexec/arm-poky-linux-gnueabi
/gcc/arm-poky-linux-gnueabi/5.2.0/real-ld: cannot find -lgcc
/opt/poky/2.0.1/sysroots/x86_64-pokysdk-linux/usr/libexec/arm-poky-linux-gnueabi
/gcc/arm-poky-linux-gnueabi/5.2.0/real-ld: cannot find -lgcc_s
/opt/poky/2.0.1/sysroots/x86_64-pokysdk-linux/usr/libexec/arm-poky-linux-gnueabi
/gcc/arm-poky-linux-gnueabi/5.2.0/real-ld: cannot find -lc
/opt/poky/2.0.1/sysroots/x86_64-pokysdk-linux/usr/libexec/arm-poky-linux-gnueabi
/gcc/arm-poky-linux-gnueabi/5.2.0/real-ld: cannot find -lgcc
/opt/poky/2.0.1/sysroots/x86_64-pokysdk-linux/usr/libexec/arm-poky-linux-gnueabi
/gcc/arm-poky-linux-gnueabi/5.2.0/real-ld: cannot find -lgcc_s
/opt/poky/2.0.1/sysroots/x86_64-pokysdk-linux/usr/libexec/arm-poky-linux-gnueabi
/gcc/arm-poky-linux-gnueabi/5.2.0/real-ld: cannot find crtend.o: No such file or
directory
/opt/poky/2.0.1/sysroots/x86_64-pokysdk-linux/usr/libexec/arm-poky-linux-gnueabi
/gcc/arm-poky-linux-gnueabi/5.2.0/real-ld: cannot find crtn.o: No such file or d
irectory
collect2: error: ld returned 1 exit status
I check file system and found crt1.o:
$ find /opt/poky/2.0.1 -name crt1.o
/opt/poky/2.0.1/sysroots/cortexa9hf-vfp-neon-poky-linux-gnueabi/usr/lib/crt1.o
Why ld can't found crt1.o and how can I solve this problem?
Thank you and excuse my bad english.
Original Attachment has been moved to: environment-setup-cortexa9hf-vfp-neon-poky-linux-gnueabi.zip
已解决! 转到解答。
Problem solved!
I add CFLAGS=""--sysroot=${SDKTARGETSYSROOT} -mfloat-abi=hard".
Where SDKTARGETSYSROOT is/ toolchain/install/directory/sysroots/cortexa9hf-vfp-neon-poky-linux-gnueabi.
Simple example:
#include <stdio.h>
int main(int argc, char *argv[]) {
return 0;
}
$ arm-poky-linux-gnueabi-gcc test.c
test.c:1:19: fatal error: stdio.h: No such file or directory
$ arm-poky-linux-gnueabi-gcc --sysroot=$SDKTARGETSYSROOT test.c
In file included from /opt/imx6_toolchain/sysroots/cortexa9hf-vfp-neon-poky-linux-gnueabi/usr/include/features.h:389:0,
from /opt/imx6_toolchain/sysroots/cortexa9hf-vfp-neon-poky-linux-gnueabi/usr/include/stdio.h:27,
from test.c:1:
/opt/imx6_toolchain/sysroots/cortexa9hf-vfp-neon-poky-linux-gnueabi/usr/include/gnu/stubs.h:7:29: fatal error: gnu/stubs-soft.h: No such file or directory
$ arm-poky-linux-gnueabi-gcc --sysroot=$SDKTARGETSYSROOT -mfloat-abi=hard test.c
$ file a.out
a.out: ELF 32-bit LSB executable, ARM, EABI5 version 1 (SYSV), dynamically linked, interpreter /lib/ld-linux-armhf.so.3, for GNU/Linux 2.6.32, BuildID[sha1]=fab88286767c018a15ba14dff125070fef88f1a4, not stripped
Hello,
perhaps the following example helps :
• Build the tool chain image. It generates the toolchain that will be installed on your host
machine and used to build any source code:
$ cd workspace/yocto/imx-4.1.15-1.0.0_ga
$ source setup-environment build-x11
$ bitbake meta-toolchain
$ cd tmp/deploy/sdk
$./fsl-imx-x11-glibc-x86_64-meta-toolchain-cortexa9hf-vfp-neon-toolchain-4.1.15-1.1.0.sh
• Hello World
$ source /opt/fsl-imx-x11/4.1.15-1.1.0/environment-setup-cortexa9hf-vfp-neonpoky-linux-gnueabi
$ cd ~/test/
$ arm-poky-linux-gnueabi-gcc helloworld.c
$ ls
a.out helloworld.c
$ ./a.out
-bash: ./a.out: cannot execute binary file
$ file a.out
a.out: ELF 32-bit LSB executable, ARM, version 1 (SYSV), dynamically linked
(uses shared libs), for GNU/Linux 2.6.16, not stripped
Have a great day,
Yuri
------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct
Answer button. Thank you!
------------------------------------------------------------------------------
Problem solved!
I add CFLAGS=""--sysroot=${SDKTARGETSYSROOT} -mfloat-abi=hard".
Where SDKTARGETSYSROOT is/ toolchain/install/directory/sysroots/cortexa9hf-vfp-neon-poky-linux-gnueabi.
Simple example:
#include <stdio.h>
int main(int argc, char *argv[]) {
return 0;
}
$ arm-poky-linux-gnueabi-gcc test.c
test.c:1:19: fatal error: stdio.h: No such file or directory
$ arm-poky-linux-gnueabi-gcc --sysroot=$SDKTARGETSYSROOT test.c
In file included from /opt/imx6_toolchain/sysroots/cortexa9hf-vfp-neon-poky-linux-gnueabi/usr/include/features.h:389:0,
from /opt/imx6_toolchain/sysroots/cortexa9hf-vfp-neon-poky-linux-gnueabi/usr/include/stdio.h:27,
from test.c:1:
/opt/imx6_toolchain/sysroots/cortexa9hf-vfp-neon-poky-linux-gnueabi/usr/include/gnu/stubs.h:7:29: fatal error: gnu/stubs-soft.h: No such file or directory
$ arm-poky-linux-gnueabi-gcc --sysroot=$SDKTARGETSYSROOT -mfloat-abi=hard test.c
$ file a.out
a.out: ELF 32-bit LSB executable, ARM, EABI5 version 1 (SYSV), dynamically linked, interpreter /lib/ld-linux-armhf.so.3, for GNU/Linux 2.6.32, BuildID[sha1]=fab88286767c018a15ba14dff125070fef88f1a4, not stripped