can not show boot message on screen

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

can not show boot message on screen

833 Views
xiaoqiangyang
Contributor III

Hi all,

Now I am working on i.MX6Q-SDP and want to show boot precess messages on LVDS.

My BSP is L3.0.35_4.1.0 and filesystem is oneiric ubuntu.

Under u-boot I use "console=ttymxc0,115200 console=tty1" but failed.Only the

serial port print messages.Removing "console=ttymxc0,115200" does not help.

How to make is work?

Besides,I want boot linux directly to text mode,not X windows.It not have

grub so I don't know how to do.I have tried disabling lightdm by editing

lightdm.conf,and I was sure it went to text mode because when I typed "reboot"

on the keyboard the board will reboot, but the screen showed nothing.

who can help me?

Any advice will be appreciated!

Best Regards

Xiaoqiang

0 Kudos
Reply
3 Replies

720 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi,

Have you tried to enable a different console? for exmaple :

console=ttymxc0,115200 console=tty2

I tried something similar in our latest BSP  and it works.

/Alejandro

0 Kudos
Reply

720 Views
xiaoqiangyang
Contributor III

Yes, I tried tty1 to tty7 but got the same result. Which version are you using?Maybe I should update my BSP.

Thanks a lot.

xiaoqiang

From: Alejandro Lozano Lozano

Date: 2015-03-18 00:56

To: Xiaoqiang Yang

Subject: Re: - can not show boot message on screen

can not show boot message on screen

reply from Alejandro Lozano Lozano in i.MX Community - View the full discussion

Hi,

Have you tried to enable a different console? for exmaple :

console=ttymxc0,115200 console=tty2

I tried something similar in our latest BSP and it works.

/Alejandro

Did your question get answered?

If so, say thanks by clicking Correct Answer in the community thread!

Reply to this message by replying to this email, or go to the message on Freescale Community

Start a new discussion in i.MX Community by email or at Freescale Community

Following can not show boot message on screen in these streams: Inbox

0 Kudos
Reply

720 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi,

I am using our latest release.

/Alejandro

0 Kudos
Reply