hi ,
I follow the newest release imx-yocto-L4.14.98_2.0.0_ga and the doc i.MX_Linux_User's_Guide.pdf to bulid gstreamer1.0-rtsp-server.
1. Enable the layer meta-openembedded/meta-multimedia:
Add the line BBLAYERS += "${BSPDIR}/sources/meta-openembedded/meta-multimedia" to the
configuration file $yocto_root/build/conf/bblayers.conf.
2. Include gst-rtsp-server into the image build:
Add the line IMAGE_INSTALL_append += "gstreamer1.0-rtsp-server" to the configuration file
$yocto_root/build/conf/local.conf.
3. Run bitbake for your image to build with gst-rstp-server.
I run build with bitbake -k core-image-minimal
but can not find :
$yocto_root/build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/gstreamer1.0-rtsp-server/$version/build/
examples/.libs
nothing can be found except for the Makfile:
ls $yocto_root/build/tmp/work/aarch64-poky-linux/gstreamer1.0-rtsp-server/1.14.4-r0/build/examples -a
. .. Makefile
when I run bitbake gstreamer1.0-rtsp-server, the same can not found .libs.
what issues I made? can anyone help me? thanks.
Hi wlxl_1204@163.com ,
To build .libs/test-uri (to build examples and tests) remove or comment the below line from file gstreamer1.0-rtsp-server.inc (path: sources/poky/meta/recipes-multimedia/gstreamer/gstreamer1.0-rtsp-server.inc).
EXTRA_OECONF = "--disable-examples --disable-tests"
then follow the steps from section 7.3.14 RTSP streaming server of i.MX Linux User's guide.
Let us know if you have any further query.
Regards,
Radhika Somaiya.