can many PCIE-device share IMX6Q's only one PCIE-BUS?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

can many PCIE-device share IMX6Q's only one PCIE-BUS?

Jump to solution
1,185 Views
翔李
Contributor IV

hi,

IMX6Q only has one PCIE bus,can i put 3 or more pcie-interface devices on this pcie bus?for example,IMX6Q---TW6869(pcie)---MINI_PCIE socket?

Labels (1)
0 Kudos
1 Solution
853 Views
igorpadykov
NXP Employee
NXP Employee

Hi 翔 李

for such purpose one can use PCIe switch like below

https://community.freescale.com/thread/324940

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
4 Replies
854 Views
igorpadykov
NXP Employee
NXP Employee

Hi 翔 李

for such purpose one can use PCIe switch like below

https://community.freescale.com/thread/324940

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
853 Views
olegpereverzev
Contributor I

I suppose you can do it implementing something like chipselect. You know, making the extension board with mcu/fpga, that will do the routing and chip selecting. You plug it in PICE, connect to several gpio pins, and it has several PCIE slots on it. When you do chip-selecting via gpio mcu/fpga do the bit stream routing to exact PCIE slot on board. Also buffer of incoming data and IRQ's. Quite a work, maybe more educated people can show you more adequate solution, don't hurry to close the question.

0 Kudos
853 Views
翔李
Contributor IV

HI,

thanks.

i need use these 3 or more pcie-device at the same time but by this only one pcie-bus of IMX6Q.Does the stabdrad protocol of PCIE allow many pcie-device directly connect to onely one pcie-bus,share one pari T,one pair R,one pair CLK?

0 Kudos
853 Views
olegpereverzev
Contributor I

IDK, but as an food for speculation

http://www.ti.com.cn/cn/lit/ds/symlink/ts2pcie412.pdf

(sorry if links to TI are not welcome here)

0 Kudos