can imx6dl deal with 2 parallel cameras ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

can imx6dl deal with 2 parallel cameras ?

408件の閲覧回数
robingcao
Contributor I

Hi ,

At first we  use imx6q to deal with the two cameras,cause it has two IPUs.

Now I want to know if imx6dl can deal the two cameras too? 

I mean one through IPU, and the another one directly send data to DDR, Could this possible ? How

ラベル(2)
0 件の賞賛
1 返信

348件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   i.MX 6DualLite has single IPU, which in its turn has two CSI (parallel) ports CSI0, CSI1.

But because of multiplexing, CSI pins may conflict with other modules ; in particular -

with (parallel) display port. Please use Pin Mux Tools to get proper configuration.

i.MX 6 Series Software and Development Tool|NXP

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛