building stressapptest for iMX6Q sabreSDP board.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

building stressapptest for iMX6Q sabreSDP board.

2,080 Views
RuchirChhabra
NXP Employee
NXP Employee

I am trying to build the stressapptest for iMX6. I am using a virtual machine to cross compile using the following command to configure.

./configure --host=arm-poky-linux-gnueabi

configure: WARNING: If you wanted to set the --build type, don't use --host.
If a cross compiler is detected then cross compile mode will be used.
configure: Compiling with dynamically linked libraries.
checking build system type... x86_64-unknown-linux-gnu
checking host system type... arm-poky-linux-gnueabi
configure: WARNING: Unsupported CPU: arm! Try x86_64, i686, powerpc, or armv7a
checking for a BSD-compatible install... /usr/bin/install -c
checking whether build environment is sane... yes
checking for arm-poky-linux-gnueabi-strip... arm-poky-linux-gnueabi-strip
checking for a thread-safe mkdir -p... /bin/mkdir -p
checking for gawk... gawk
checking whether make sets $(MAKE)... yes
checking for arm-poky-linux-gnueabi-g++... arm-poky-linux-gnueabi-g++
checking whether the C++ compiler works... no
configure: error: in `/home/r2aaje/Documents/stressapptest':
configure: error: C++ compiler cannot create executables
See `config.log' for more details.

 

I get the warning highlighted in red above. Any idea on why that is? Has anyone build this app successfully and run on the iMX sabre boards?

Original Attachment has been moved to: config.log.zip

Labels (2)
0 Kudos
Reply
3 Replies

1,394 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Ruchir,

Per you issue looks more like you are working with the incorrect version of your tool or arm architecture is not supported in that tool, however Please try to use the official NXP i.MX6 DDR stress test tool:

i.MX6/7 DDR Stress Test Tool V2.52 

regards

0 Kudos
Reply

1,394 Views
RuchirChhabra
NXP Employee
NXP Employee

Thanks for the reply. I need run both DDR stress test and the stressapptest on the same board. Issue is how to setup the config file to cross compile successfully.

0 Kudos
Reply

949 Views
jekim
Contributor III

Hello,

 

If the "stressapptest" is working on your board, could you let me know how the configuration should be set? Thanks.

 

Best Regards,

Jeff

0 Kudos
Reply