hi,
I followed the below instructions for building the ivi image for my board(imx6qpsabre auto).
Build instructions:
Install the `repo` utility:
$: mkdir ~/bin
$: curl http://commondatastorage.googleapis.com/git-repo-downloads/repo > ~/bin/repo
$: chmod a+x ~/bin/repo
$: PATH=${PATH}:~/bin
Download the BSP Yocto Project Environment
$: mkdir fsl-arm-yocto-bsp
$: cd fsl-arm-yocto-bsp
$: repo init -u http://sw-stash.freescale.net/scm/imx/fsl-arm-yocto-bsp.git -b imx-4.1.15-1.0.0_genivi-demo
$: repo sync
Setup and Build for Wayland
$: DISTRO=nxp-imx-genivi-wayland MACHINE=imx6qsabreauto source nxp-setup-genivi.sh -b build-genivi
Basic image for genivi:
$: bitbake leviathan-image
$: bitbake ivi-image.
bitbake fsl-image-qt5.
I am able to build but when try to run the image on the board.
ie.:sudo dd if=fsl-image-qt5.sdcard of=/dev/sdb bs=1M&&sync : and booted board from the sd card.
I am getting the bellow errors couldn't get the handle stuck in the middle .
errors: check the images.
Please suggest me correct ivi build procedure to run on the imx6qp sabre ai board.
Regards,
Lavakumar S
Helo Lavakumar S,
I’m trying to replicate this issue but I’m seeing fetching errors when baking the leviathan-image.
Are you still having this issue? I cannot replicate it but I would think the baking was correct as it finished without errors on your side. However, it is possible that the loading of the image to the SD card wasn’t finished correctly. The dd instruction seems correct, but sometimes the sync after the dd does not work and the partition table is corrupted. I would recommend trying again and synching manually (alternatively you may restart the host to force the kernel to update the partition table).
I hope this helps!
Regards,
hi gusarambula,
Thanks for your reply.
I also faced the same issue and followed " http://git.freescale.com/git/cgit.cgi/imx/fsl-arm-yocto-bsp.git/tree/README?h=imx-4.1.15-1.0.0_gathis " url to download and succeeded.
Please check and reply.
Regards,
Lavakumar S
hi,
Yes.
I am able to build fsl-image-qt5 and leviathan-image. those errors I am getting for leviathan image .
Those errors comes only with the build package with meta-ivi layer.
Thanks
Regards,
Lavakumar S
Hello Lavakumar S
Are you still experiencing issues with this image?
The link I was given for the instructions on building the GENIVI image is:
http://git.freescale.com/git/cgit.cgi/imx/meta-nxp-genivi.git/tree/README.txt
I had some problems when baking and I haven't been able to bake the image and test it but perhaps you may.
Regards,
hi gusarambula,
yes the issues still there but kernel is alive so that I can process further.
and I bitbaked leviathan-mage. not the Miranda-image.
why cant you bake it ? I think I used some pre downloaded packages as well.
regards,
Lavakumar S