hi ,
i am trying to build the sources for i.MX8 nano facing the below issue.
OTE: Setscene tasks completed
WARNING: libarchive-native-3.4.0-r0 do_fetch: Failed to fetch URL http://libarchive.org/downloads/libarchive-3.4.0.tar.gz, attempting MIRRORS if available
ERROR: libarchive-native-3.4.0-r0 do_fetch: Fetcher failure: Fetch command export PSEUDO_DISABLED=1; unset _PYTHON_SYSCONFIGDATA_NAME; export DBUS_SESSION_BUS_ADDRESS="unix:path=/run/user/1001/bus"; export SSH_AGENT_PID="1557"; export SSH_AUTH_SOCK="/run/user/1001/keyring/ssh"; export PATH="/home/edttesting/nxp/i.MX8/imx-yocto-bsp/sources/poky/scripts/native-intercept:/home/edttesting/nxp/i.MX8/imx-yocto-bsp/sources/poky/scripts:/home/edttesting/nxp/i.MX8/imx-yocto-bsp/build/tmp/work/x86_64-linux/libarchive-native/3.4.0-r0/recipe-sysroot-native/usr/bin/x86_64-linux:/home/edttesting/nxp/i.MX8/imx-yocto-bsp/build/tmp/work/x86_64-linux/libarchive-native/3.4.0-r0/recipe-sysroot-native/usr/bin:/home/edttesting/nxp/i.MX8/imx-yocto-bsp/build/tmp/work/x86_64-linux/libarchive-native/3.4.0-r0/recipe-sysroot-native/usr/sbin:/home/edttesting/nxp/i.MX8/imx-yocto-bsp/build/tmp/work/x86_64-linux/libarchive-native/3.4.0-r0/recipe-sysroot-native/usr/bin:/home/edttesting/nxp/i.MX8/imx-yocto-bsp/build/tmp/work/x86_64-linux/libarchive-native/3.4.0-r0/recipe-sysroot-native/sbin:/home/edttesting/nxp/i.MX8/imx-yocto-bsp/build/tmp/work/x86_64-linux/libarchive-native/3.4.0-r0/recipe-sysroot-native/bin:/home/edttesting/nxp/i.MX8/imx-yocto-bsp/sources/poky/bitbake/bin:/home/edttesting/nxp/i.MX8/imx-yocto-bsp/build/tmp/hosttools"; export HOME="/home/edttesting"; /usr/bin/env wget -t 2 -T 30 --passive-ftp --no-check-certificate -P /home/edttesting/nxp/i.MX8/imx-yocto-bsp/downloads/ 'http://libarchive.org/downloads/libarchive-3.4.0.tar.gz' --progress=dot -v failed with exit code 4, output:
--2021-04-01 10:32:56-- http://libarchive.org/downloads/libarchive-3.4.0.tar.gz
Resolving libarchive.org (libarchive.org)... 13.227.166.74, 13.227.166.89, 13.227.166.116, ...
Connecting to libarchive.org (libarchive.org)|13.227.166.74|:80... connected.
HTTP request sent, awaiting response... Read error (Connection timed out) in headers.
Retrying.
--2021-04-01 10:33:27-- (try: 2) http://libarchive.org/downloads/libarchive-3.4.0.tar.gz
Connecting to libarchive.org (libarchive.org)|13.227.166.74|:80... connected.
HTTP request sent, awaiting response... Read error (Connection timed out) in headers.
Giving up.
ERROR: libarchive-native-3.4.0-r0 do_fetch: Fetcher failure for URL: 'http://libarchive.org/downloads/libarchive-3.4.0.tar.gz'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /home/edttesting/nxp/i.MX8/imx-yocto-bsp/build/tmp/work/x86_64-linux/libarchive-native/3.4.0-r0/temp/log.do_fetch.418975
ERROR: Task (virtual:native:/home/edttesting/nxp/i.MX8/imx-yocto-bsp/sources/poky/meta/recipes-extended/libarchive/libarchive_3.4.0.bb:do_fetch) failed with exit code '1'
NOTE: Tasks Summary: Attempted 788 tasks of which 506 didn't need to be rerun and 1 failed.
Summary: 1 task failed:
virtual:native:/home/edttesting/nxp/i.MX8/imx-yocto-bsp/sources/poky/meta/recipes-extended/libarchive/libarchive_3.4.0.bb:do_fetch
Summary: There were 2 WARNING messages shown.
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.
Thank you,
Y Mahesh.
Hi Israel,
thanks for responding.
please find the below steps.
$ mkdir imx-yocto-bsp
$ cd imx-yocto-bsp
$ repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-zeus -m imx-5.4.47-2.2.0.xml
$ repo sync
$ DISTRO=fsl-imx-xwayland MACHINE=imx8mnevk source imx-setup-release.sh -b build
$ bitbake imx-image-full
Thank you,
Y Mahesh.
Hi Mahesh27,
I tried to replicate the error that you have without success, sometimes this kind of error happens when the data can't be retrieved from the source, so usually rebuilding the image again it works, also try to update the programs too, just to be sure that we do not have issues with that.
Regards,
Israel.