boot from nand

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

boot from nand

2,197件の閲覧回数
enaud
Contributor III

Hi,

how is possible flash nand (with uboot.bin, uImage and rootfs) and start without SD but only from nand?

thanks

ラベル(1)
0 件の賞賛
返信
7 返答(返信)

1,735件の閲覧回数
enaud
Contributor III

QSB

0 件の賞賛
返信

1,735件の閲覧回数
KrishnaPavan
Contributor II

Is it QSB or SABRE or ARD or EVK etc etc.?

enaud said:

imx53

0 件の賞賛
返信

1,735件の閲覧回数
enaud
Contributor III

imx53

0 件の賞賛
返信

1,735件の閲覧回数
KrishnaPavan
Contributor II

Which board are you using?

0 件の賞賛
返信

1,735件の閲覧回数
DirkBehme
Contributor III

You might want to have a look to

http://imxcommunity.org/forum/topics/cannot-boot-from-nand

The discussion there is about the i.MX53 ARD board, but some parts might help for the QSB, too.

0 件の賞賛
返信

1,735件の閲覧回数
positron
Contributor I

Hello, Not only the hardware connection. You need to change the imximage.cfg (for u-boot) configurations to make it boot from NAND. If you are looking for a one-line answer on how to boot from NAND, I'd say "It is not that easy". You need to study the manual, patch in the IOMUX settings, write imximage.cfg, tweak the board file. Do it one step at a time.

0 件の賞賛
返信

1,734件の閲覧回数
jomeke
Contributor II

Hi Enaud,

you can find the information in the user manual under chapter 7.

I have made a summary in the Excel file attached.

Have a look

0 件の賞賛
返信