bitbake core-image-base:Unable to start bitbake server

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

bitbake core-image-base:Unable to start bitbake server

3,185 Views
1844350626
Contributor I

Hello all,

The problem as below:

Step 1: DISTRO=fsl-imx-fb MACHINE=imx7dsabresd source imx-setup-release.sh -b fsl-imx-fb

Step 2: cd fsl-imx-fb 

Step 3:bitbake core-image-base

After a whole night,report error and exit.

step 4::bitbake core-image-base

Now report error as below:

ERROR: Unable to start bitbake server (None)
ERROR: Server log for this session (/work/yocto/fsl-imx-fb/bitbake-cookerdaemon.log):
--- Starting bitbake server pid 80094 at 2020-12-02 09:04:22.952896 ---
ERROR: Layer freescale-layer is not compatible with the core layer which only supports these series: zeus (layer is compatible with hardknott gatesgarth)

Labels (1)
0 Kudos
Reply
1 Reply

3,179 Views
joanxie
NXP TechSupport
NXP TechSupport

after you use the command

“ DISTRO=fsl-imx-fb MACHINE=imx7dsabresd source imx-setup-release.sh -b fsl-imx-fb”, you should already enter the folder fsl-imx-fb, so if you do the step2, you should get error, didn't you get anything wrong? and did you repo sync successfully? and tell me what bsp version you built?

 

 

0 Kudos
Reply