autorun-vpu.sh

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

autorun-vpu.sh

Jump to solution
1,071 Views
grim
Contributor III

I'm trying to test the VPU in my system and every time I run 'autorun-vpu.sh' I get the following output.

root@imx6solosabresd:/unit_tests# ./autorun-vpu.sh

Checking for devnode: /dev/mxc_vpu

autorun-vpu.sh: PASS devnode found: /dev/mxc_vpu

Running test case: ./mxc_vpu_test.out -C config_dec

/unit_tests/test-utils.sh: line 11: ./mxc_vpu_test.out: No such file or directory

autorun-vpu.sh: FAIL test case: ./mxc_vpu_test.out -C config_dec

autorun-vpu.sh: Exiting FAIL

It doesn't seem to matter if I run this on a SabreSD board, our custom imx6 solo or imx6 quad board.

I built the binaries with Fido distribution of Yocto (fsl-image-machine-test).

All of the other tests I've ran seem to work.... except for this one.

Anybody else have this issue? How did you get around it?

Labels (4)
1 Solution
854 Views
grim
Contributor III

I'm assuming this doesn't work because of some configuration error.

Running from a pre-built image seems to yield better results.

View solution in original post

0 Kudos
Reply
3 Replies
853 Views
igorpadykov
NXP Employee
NXP Employee

Hi Bob

please try to build fsl-image-gui or fsl-image-qt5

image as shows attached Yocto Guide Table 1. Freescale Yocto project images,

use imx6qsabresd machine configuration. Other way use Demo images

from L3.14.28_1.0.0_iMX6QDLS_BUNDLE.

Board Support Packages (27)

L3.14.28_1.0.0_iMX6QDLS_BUNDLE (REV L3.14.28_1.0.0)

i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo Linux Binary Demo Files and Linux BSP Documentation

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREBRD&fpsp=1&tab=Design_Tool...

Best regards

igor

853 Views
vikaspatil
Senior Contributor I

I am facing the same issue. What configuration option  I need to set. It works on our custom target if i use it from  fsl-image-qt5 build.

Regards,

Vikash

0 Kudos
Reply
855 Views
grim
Contributor III

I'm assuming this doesn't work because of some configuration error.

Running from a pre-built image seems to yield better results.

0 Kudos
Reply