arecord aplay loop-back test in iMX6ULL evk board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

arecord aplay loop-back test in iMX6ULL evk board

4,808件の閲覧回数
mannsikchung
Contributor III

Dear All

arecord (MIC) is not working.

How can I enable MIC?

I'm using iMX6ULL14x14evk board and build SD image using bitbake core-image-sato.

Before bitbake core-image-sato, I added alsa-utils in conf/local.conf as below.

$ vi conf/local.conf

...

CORE_IMAGE_EXTRA_INSTALL += "\
 alsa-utils"

After boot completed I checked aplay is working using "aplay my.wav".
But, I coundn't make arecord work.

I tried below command but loop-back sound not played.

root@imx6ull14x14evk:~# arecord -D hw:0,0 -f cd | aplay
Recording WAVE 'stdin' : Signed 16 bit Little Endian, Rate 44100 Hz, Stereo
Playing WAVE 'stdin' : Signed 16 bit Little Endian, Rate 44100 Hz, Stereo

In my guess MIC is not working. So, I tried another evk( I have two iMX6ULL evk boards). But, same as before, no loop-back.

Below is full build and test snippets.
Please let me know my missing.

[In Ubuntu Development Host PC]

$ repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-4.1-krogoth -m imx-4.1.15-2.0.3.xml
$ repo sync

$ MACHINE=imx6ull14x14evk source fsl-setup-release.sh -b build

$ vi conf/local.conf

.... 

CORE_IMAGE_EXTRA_INSTALL += "alsa-utils"

$ bitbake core-image-sato

[After EVK boot completed]

root@imx6ull14x14evk:~# arecord -l
**** List of CAPTURE Hardware Devices ****
card 0: wm8960audio [wm8960-audio], device 0: HiFi wm8960-hifi-0 []
  Subdevices: 1/1
  Subdevice #0: subdevice #0
card 0: wm8960audio [wm8960-audio], device 1: HiFi-ASRC-FE (*) []
  Subdevices: 1/1
  Subdevice #0: subdevice #0

root@imx6ull14x14evk:~# arecord -D hw:0,0 -f cd | aplay
Recording WAVE 'stdin' : Signed 16 bit Little Endian, Rate 44100 Hz, Stereo
Playing WAVE 'stdin' : Signed 16 bit Little Endian, Rate 44100 Hz, Stereo

But, No Loop-Back Sound.

I tried below list aslo

  • arecord without -D option but no loop-bake sound..
  • arecord with -D hw:0,1 option but no loop-bake sound..
  • arecord without -f option but no loop-bake sound..
  • test above in bitbake fsl-image-gui image also, but no loop-bake sound.

Best Regards

Mannsik

ラベル(5)
タグ(3)
6 返答(返信)

2,916件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Please use section 28.5 (Unit Test) of i.MX Linux® Reference Manual (Rev. 0, 10/2016).

For i.MX 6UL EVK, there are two analog microphones, MAIN MIC and HP MIC.
MAIN MIC is connected to the RINPUT1 and RINPUT2 ports to support differential
microphone. HP MIC is connected to the LINPUT1 and LINPUT3 ports. To enable
the analog microphone, execute the following amixer commands:
• amixer cset name='Left Input Mixer Boost Switch' on
• amixer cset name='Left Boost Mixer LINPUT1 Switch' on
• amixer cset name='Left Boost Mixer LINPUT2 Switch' on
• amixer cset name='Left Boost Mixer LINPUT3 Switch' on
• amixer cset name='Right Input Mixer Boost Switch' on
• amixer cset name='Right Boost Mixer RINPUT1 Switch' on
• amixer cset name='Right Boost Mixer RINPUT2 Switch' on
• amixer cset name='Right Boost Mixer RINPUT3 Switch' off
• amixer cset name='ADC PCM Capture Volume' 220

By default, for HP MIC and MAIN MIC, only one channel has voice when recording
stereo WAV (Left Data = Left ADC; Right Data = Right ADC):
• amixer cset name='ADC Data Output Select' 0

When using HP MIC to support stereo, route the left ADC date to the right ADC
channel (Left Data = Left ADC; Right Data = Left ADC):
• amixer cset name='ADC Data Output Select' 1

When using MAIN MIC to support stereo, route the right ADC date to the left ADC
channel (Left Data = Right ADC; Right Data = Right ADC):
• amixer cset name='ADC Data Output Select' 2

The record feature can be tested by the following command:
• arecord [-Dplughw:0,0] -r 44100 -f S16_LE -c 2 -d 5 record.wav

More usages for aplay/arecord/amixer can be obtained by the following commands:
• aplay --h
• arecord --h
• amixer --h

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,653件の閲覧回数
sicScar7
Contributor I

Hi there!

I manage to enable the ON BOARD MIC for i.MX6ULL EVK.

This sequence worked for me (as yuri solution), I post it as shell script:

 

#!/bin/bash

echo "Enabling on board MIC for i.MX6ULL EVK"

amixer cset name='Left Input Mixer Boost Switch' on
amixer cset name='Left Boost Mixer LINPUT1 Switch' on
amixer cset name='Left Boost Mixer LINPUT2 Switch' on
amixer cset name='Left Boost Mixer LINPUT3 Switch' on
amixer cset name='Right Input Mixer Boost Switch' on
amixer cset name='Right Boost Mixer RINPUT1 Switch' on
amixer cset name='Right Boost Mixer RINPUT2 Switch' on
amixer cset name='Right Boost Mixer RINPUT3 Switch' off
amixer cset name='ADC PCM Capture Volume' 220
amixer cset name='ADC Data Output Select' 0

 

just test it easily with :

arecord -f cd -d 10 record.wav

aplay record.wav   

 

(I used this forum too many times to not help other people )

See ya

0 件の賞賛
返信

2,916件の閲覧回数
thisseemsbroken
Contributor I

Hate to come in the middle of things like this.   I'm trying to use a mic on J1401, and not getting any sound.  Tried turning off all of [LR]INPUT[123] except LINPUT3.  It's been some time since doing this at the a[lsa]mixer level, and suspect that I'm missing something really obvious.  How do I get HP_MIC to work?

2,916件の閲覧回数
mannsikchung
Contributor III

Please help me, if you get working let me know How to do it.
Still I have no idea of how to get MIC working.

0 件の賞賛
返信

2,916件の閲覧回数
mannsikchung
Contributor III

Hi Yuri

Thank you for your response.

But, with your suggestion of using amixer, I couldn't record voice over MIC.

First of all, I'm using iMX6ULL(double L) evk not iMX6UL.

I changed lot's of settings in alsamixer also, but, I couldn't record.

Is there any difference between --ULL and UL?

BR.

Mannsik

0 件の賞賛
返信

2,916件の閲覧回数
Yuri
NXP Employee
NXP Employee
0 件の賞賛
返信