各位尊敬的FAE:
我遇到一个情况。首先使用mfgtool烧录你们的android7.1.1镜像到 官方i.MX 6Quad 开发板,可以使用。但是因为我们最终需要运用到自己的板子上,一定会需要修改mfgtool下uboot和kernel。之前看过如何获得mfgtool下的u-boot-imx6dlsabresd_sd.imx?不需要单独为mfgtool编译uboot。所以尝试将u-boot-imx6q.imx拷贝到firmware下重命名为u-boot-imx6qsabresd_sd.imx,但是在烧录的时候卡住,串口日志如下。mfgtool的log在附件
U-Boot 2015.04 (Feb 17 2017 - 12:07:45)
CPU: Freescale i.MX6Q rev1.2 at 792 MHz
CPU: Temperature 34 C
Reset cause: POR
Board: MX6-SabreSD
I2C: ready
DRAM: 1 GiB
PMIC: PFUZE100 ID=0x10
MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
MMC: no card present
MMC init failed
Using default environment
No panel detected: default to Hannstar-XGA
Display: Hannstar-XGA (1024x768)
In: serial
Out: serial
Err: serial
unsupported boot devices
SATA isn't buildin
MMC: no card present
Block device mmc 0 not supported
rw_block, get_block_size return 0
read_bootctl, rw_block read failed
read command failed
Fastboot: Normal
Net: FEC [PRIME]
MMC: no card present
Block device mmc 0 not supported
rw_block, get_block_size return 0
read_bootctl, rw_block read failed
read command failed
=>
Original Attachment has been moved to: MfgTool.log.zip
不需要单独编译 firmware的uboot。 就是 firmware 和正常使用的uboot 是共享一个的。
但不是说可以用 参考板的uboot,也是需要根据你的板子修改出来的uboot的。
记得做你的板子的DDR 校准并且apply 到uboot 的 DCD 里面。
移植先做好。
如果不用PMIC, 就用ldo enable的device tree
这个文档说了 为什么 mfg tool 的uboot 和 平时用的uboot 是一个。
i.MX Development Miscellanea(i.MX 开发杂记)
https://community.nxp.com/docs/DOC-335198
MFGTool_Uboot_share_with_NormalRun_sourceCode.pdf
Hi,
Have you changed the DDR design in your board design? If no, you can use the mfgtool provide by NXP. You need to porting BSP and build the images for your board.
From you above information, you copy your u-boot file to firmware, the name must be same in ucl2.xml script. You can check it first. The download images to your board process is following the script.
Have a great day,
Rita
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
我自己的板子是变化了的,但是上面的操作我都是在官方demo板上做的。ucl2.xml我就是依据它,改名替换的firmware的uboot。而且如果替换的不正确,对烧录不会产生影响,我现在烧录不了,应该是替换对了的。
</LIST>
<LIST name="eMMC-Android" desc="Choose eMMC as media">
<CMD state="BootStrap" type="boot" body="BootStrap" file ="firmware/u-boot-imx6q%plus%%board%_sd.imx" ifdev="MX6Q">Loading U-boot</CMD>