android4.4.2将tablet更改为phone

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

android4.4.2将tablet更改为phone

3,082件の閲覧回数
ninglu
Contributor II

你好:

    我们的平台是android4.4.2,  imx6dq,linux3.0.35.

    我想将在关机或其他界面上出现的tablet(平板电脑)等字符换成phone(手机),是不是要设置ro.build.characteristics或PRODUCT_CHARACTERISTICS。

我将build.prop在中的ro.build.characteristics设置成了default,将device/fsl/imx6/sabresd_6q.mk文件中的PRODUCT_CHARACTERISTICS := tablet改为

PRODUCT_CHARACTERISTICS := default。

编译后下载到板子上,但是关机时,仍然显示的是您的平板电脑会关闭。

请问需要在哪里修改呢

ラベル(5)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

1,881件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

have you try change to PRODUCT_CHARACTERISTICS := phone ?

0 件の賞賛
返信

1,881件の閲覧回数
ninglu
Contributor II

我试过将PRODUCT_CHARACTERISTICS := phone ,但是还是不行,依然显示 平板电脑,

还有别的地方设置了吗?

luning@huadong.net

发件人: jimmychan

发送时间: 2016-07-14 15:56

收件人: nin lu

主题: Re: - android4.4.2将tablet更改为phone

NXP Community

android4.4.2将tablet更改为phone

reply from jimmychan in i.MX Community - View the full discussion

have you try change to PRODUCT_CHARACTERISTICS := phone ?

Reply to this message by replying to this email, or go to the message on NXP Community

Start a new discussion in i.MX Community by email or at NXP Community

Following android4.4.2将tablet更改为phone in these streams: Inbox

This email was sent by NXP Community because you are a registered user.

You may unsubscribe instantly from NXP Community, or adjust email frequency in your email preferences

0 件の賞賛
返信

1,881件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

In build/tools/buildinfo.sh, ro.build.characteristics is = $TARGET_AAPT_CHARACTERISTICS.

So, you can try to modify the build/core/product_config.mk. Change the setting for TARGET_AAPT_CHARACTERISTICS to 'default'.  After built success, you can check the value of  ro.build.characteristics in build.prop again.

0 件の賞賛
返信