android r10.3.1 for QSB dual video output issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

android r10.3.1 for QSB dual video output issue

579件の閲覧回数
JackyHuang
Contributor III

Now I have patched the android r10.3.1 to the android r10.3 base source .

when I test the dual video function, I found that it can't work

only one screen show the video as well as the screen is flicker

the property setup as below:

[rw.secfb.disable-overlay]: [1]
[rw.SIN_VIDEO_DUAL_UI]: [0]
[rw.DUAL_VIDEO_SIN_UI]: [1]

[rw.SECOND_DISPLAY_CONNECTED]: 1
[sys.SECOND_DISPLAY_ENABLED]: 1

but when I set the [rw.secfb.disable-overlay] to 0, the screen no flicker any more, but still one screen show the video.

Are there any kernel option I haven't choosed.

Thanks you help advance!

タグ(1)
0 件の賞賛
1 返信

422件の閲覧回数
JackyHuang
Contributor III

Yesterday,  I use the mx51 bbg run the r10.3.1 and try to make the dual video output work.

However, the video only output to the primary screen,

Is it impossible archive dual video output on r10.3.1?

0 件の賞賛