Hi,
I want to run android_kk4.4.2 in my imx6Q (MCIMX6Q-SDP) demo board. When I tried to boot from my SD card
with pre-built image (android_kk4.4.2_1.0.0-ga_full_image_6qsabresd - downloaded from freescale site) , the boot process was unable to complete and booted till the "android" logo
and then it is stuck after that.
Please put your suggestions.
NOTE: I have used an 8GB SD card formatted as per the android user guide in freescale site.
please help me to fix this problem.
Hi Roopesh,
I think your android booting is stopping on the framework issue.
Please connect the USB<->UART wire to your PC and provide the log from console.
If possible you can type in "logcat -v time" and copy the logcat of Android for debugging.
Thanks
BRs,
Haoran
Hi SerchMX,
Thanks for your interest.
I used the following command to download the image to SD card. The SD card was partitioned using mksdcard-android.sh /dev/sdb
sudo dd if=u-boot-6q.bin of=/dev/sdb bs=1K skip=1 seek=1; sync
sudo dd if=boot.img of=/dev/sdb1; sync
sudo dd if=system.img of=/dev/sdb5; sync
sudo dd if=recovery.img of=/dev/sdb2; sync
As the board stuck at android logo during boot up , I didn't get any error logs or messages.
Also I have configured the board ( SW6) according to the user guide.
MMC2(SD3) boot - (SW6) 01000010
Regards,
Roopesh