Hi, gentlemen
I am debugging adv7180 in imx6solo platform, after configuration, the image can be captured, but it is not correct, it seems like combination of 2 frames, please refer to attachments(a bmp file and a raw data file).
The BSP version is 4.1.15, the configuration in dts file is as follow, and the source code of ADV7180 is in the attachments.
&i2c1 {
adv7180: adv7180@20 {
compatible = "adv,adv7180";
reg = <0x20>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_ipu1_2>;
csi_id = <0>;
cvbs = <1>;
};
};
Any advice would be appreciated.
Winbo.
Original Attachment has been moved to: image.yuv.zip
Original Attachment has been moved to: adv7180.c.zip
it seems you don't de-interlacing, you can refer to the link as below, compare what you set
This issue has been solved. The reason is that I use an capture application download from web, after trying mxc_v4l2_tvin.out, it's ok. Thanks anyway.
Best regards.
Winbo