Hi, i have same question about adv7181display on screen,
1 . Now I use Yocto project "imx6q_L3_14_52" & "fsl-releases-bsp";
2. CVBS signal through adv7181converts to bt656,and V4l2 capture image and display on LCD;
The quetsion is the display and capture iimage have some Horizontal stripes,for examples please look the attachment,and how about to slove it ? thanks!
Hi rothwan
for bt656 camera format mxc_v4l2_tvin.c should be used,
not V4l2 capture, please test with imx-test/test/mxc_v4l2_test
www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.3.tar.gz
Also stripes may be caused by resizing, please check
i.MX6 GStreamer-imx Plugins - Tutorial & Example Pipelines
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Some people think that is the conversion, the singal of CVBS is interleave,and the signal from adv7181 is the interleave,but imx6q the display is progressive,If this problem causes, how to solve?
Yes, i have check it , and For adv7181, I have try the followed settting:
p->if_type = V4L2_IF_TYPE_BT656;
p->u.bt656.mode = V4L2_IF_TYPE_BT656_MODE_NOBT_8BIT;
p->u.bt656.nobt_hs_inv = 0;
p->u.bt656.bt_sync_correct = 0; // Use internal VSYNC mode, CSI_VSYNC and CSI_HSYNC pins are not needed.
p->u.bt656.clock_curr = 0; //BT656 interlace clock mode
adv7181 I2C register setting for CVBS input:
adv7180_write_reg(0x00,0x00);
adv7180_write_reg(0x03,0x0c);
adv7180_write_reg(0x04,0x77);
adv7180_write_reg(0x17,0x41);
adv7180_write_reg(0x1d,0x47);
adv7180_write_reg(0x31,0x02);
adv7180_write_reg(0x3a,0x17);
adv7180_write_reg(0x3b,0x81);
adv7180_write_reg(0x3d,0xa2);
adv7180_write_reg(0x3e,0x6a);
adv7180_write_reg(0x3f,0xa0);
adv7180_write_reg(0x86,0x0b);
adv7180_write_reg(0xf3,0x01);
adv7180_write_reg(0xf9,0x03);
adv7180_write_reg(0x0e,0x80);
adv7180_write_reg(0x52,0x46);
adv7180_write_reg(0x54,0x00);
adv7180_write_reg(0x7f,0xff);
adv7180_write_reg(0x81,0x30);
adv7180_write_reg(0x90,0xc9);
adv7180_write_reg(0x91,0x40);
adv7180_write_reg(0x92,0x3c);
adv7180_write_reg(0x93,0xca);
adv7180_write_reg(0x94,0xd5);
adv7180_write_reg(0xb1,0xff);
adv7180_write_reg(0xb6,0x08);
adv7180_write_reg(0xc0,0x9a);
adv7180_write_reg(0xcf,0x50);
adv7180_write_reg(0xd0,0x4e);
adv7180_write_reg(0xd1,0xb9);
adv7180_write_reg(0xd6,0xdd);
adv7180_write_reg(0xd7,0xe2);
adv7180_write_reg(0xe5,0x51);
adv7180_write_reg(0xf6,0x3b);
adv7180_write_reg(0x0e,0x00);
but this problem is still ,Why?