After building an image out of
repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-sumo -m imx-4.14.78-1.0.0_ga.xml
build on 8qm machine
MACHINE=imx8qmmek DISTRO=fsl-imx-xwayland source ./fsl-setup-release.sh -b bld-xwayland
the image can't boot ...
sudo dd if=core-image-minimal-imx8qmmek.sdcard of=/dev/mmcblk0 bs=1M conv=fsync
I can build core-image-minimal
bitbake core-image-minimal
There is no problem to build but after flashing on sdcard that sdcard image (core-image-minimal) is not booting ...
I showed all procedure I am doing above.