Hi,
Sorry if it is a repeated question but could not find this specific issue mentioned before.
Trying to bitbake yocto sdk 1.1.1 2.4 under Ubuntu 16.04:
2123 mkdir yocto-sdk
2124 cd yocto-sdk/
2126 sudo ~/bin/repo init -u https://source.codeaurora.org/external/qoriq/qoriq-components/yocto-sdk -b thud
2129 sudo ~/bin/repo sync --no-clone-bundle
2130 . ./setup-env -m t4240rdb-64b
2131 bitbake fsl-image-networking
and seeing this error:
ERROR: bzip2-native-1.0.6-r5 do_fetch: Fetcher failure for URL: 'http://downloads.yoctoproject.org/mirror/sources/bzip2-1.0.6.tar.gz'. Unable to fetch URL from any source.
ERROR: bzip2-native-1.0.6-r5 do_fetch: Function failed: base_do_fetch
Looking at the log:
Resolving downloads.yoctoproject.org (downloads.yoctoproject.org)... 198.145.29.63
Connecting to downloads.yoctoproject.org (downloads.yoctoproject.org)|198.145.29.63|:80... connected.
HTTP request sent, awaiting response... 200 OK
Length: 782025 (764K) [application/octet-stream]
Saving to: ...Downloads/yocto-sdk/downloads/bzip2-1.0.6.tar.gz’
0K .......... .......... .......... .......... .......... 6% 272K 3s
50K .......... .......... .......... .......... .......... 13% 518K 2s
100K .......... .......... .......... .......... .......... 19% 297K 2s
150K .......... .......... .......... .......... .......... 26% 87.7K 3s
200K .......... .......... .......... .......... .......... 32% 449K 2s
250K .......... .......... .......... .......... .......... 39% 9.60M 2s
300K .......... .......... .......... .......... .......... 45% 18.2M 1s
350K .......... .......... .......... .......... .......... 52% 262K 1s
400K .......... .......... .......... .......... .......... 58% 2.84M 1s
450K .......... .......... .......... .......... .......... 65% 367K 1s
500K .......... .......... .......... .......... .......... 72% 3.16M 1s
550K .......... .......... .......... .......... .......... 78% 4.75M 0s
600K .......... .......... .......... .. 82% 15.8M=1.5s
2019-03-13 19:33:12 (419 KB/s) - Read error at byte 647168/782025 (Success). Retrying.
--2019-03-13 19:33:13-- (try: 2) http://downloads.yoctoproject.org/mirror/sources/bzip2-1.0.6.tar.gz
Connecting to downloads.yoctoproject.org (downloads.yoctoproject.org)|198.145.29.63|:80... connected.
HTTP request sent, awaiting response... 206 Partial Content
Length: 782025 (764K), 134857 (132K) remaining [application/octet-stream]
Saving to: ...Downloads/yocto-sdk/downloads/bzip2-1.0.6.tar.gz’
[ skipping 600K ]
600K ,,,,,,,,,, ,,,,,,,,,, ,,,,,,,,,, ,,........ ....... 84% 11.4M=0.001s
2019-03-13 19:33:45 (11.4 MB/s) - Read error at byte 663292/782025 (Success). Giving up.
ERROR: Fetcher failure for URL: 'http://downloads.yoctoproject.org/mirror/sources/bzip2-1.0.6.tar.gz'. Unable to fetch URL from any source.
The odd thing is that looking here: "http://downloads.yoctoproject.org/mirror/sources/"
I can download several files of various sizes but not the bzip2-1.0.6... in question. There are probably other files that fail as well. It seems like a server problem to me but that seems odd.
Thanks,
Tomas
NXP offers SDK 2.0 Yocto based Linux BSP for the T4240rdb board:
We have tested this SDK under Ubuntu 12 and Ubuintu 14t. Do not use Ubuntu 16.
Use the following command sequence:
Message: /bin/sh -> dash
Answer after password – No
Message:
Removing 'diversion of /bin/sh to /bin/sh.distrib by dash'
Adding 'diversion of /bin/sh to /bin/sh.distrib by bash'
Removing 'diversion of /usr/share/man/man1/sh.1.gz to /usr/share/man/man1/sh.distrib.1.gz by dash'
Adding 'diversion of /usr/share/man/man1/sh.1.gz to /usr/share/man/man1/sh.distrib.1.gz by bash'
Message: /bin/sh -> bash
Usually Linux recommends also run the following command: sudo usr/sbin/visudo
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------