Yocto Marvell 88e6xxx driver

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Yocto Marvell 88e6xxx driver

486件の閲覧回数
MJaroc
Contributor II

Hi,

i attach marvell switch to board, configure it in device tree:

&mdio1 {
 #address-cells = <1>;
 #size-cells = <0>;
 
 switch0: switch0@0 {
	compatible = "marvell,mv88e6085";
	reg = <0>;
	dsa,member = <0 0>;

 	ports {
	 	#address-cells = <1>;
		#size-cells = <0>;
		port@0 {
			reg = <0>;
			label = "lan0";
			fixed-link {
				speed = <1000>;
				full-duplex;
			};			
		};
        
		port@1 {
			reg = <1>;
			label = "lan1";
			fixed-link {
				speed = <1000>;
				full-duplex;
			};
		};
		
		port@3 {
			reg = <3>;
			label = "nmi";
		};

		switch0cpu5: port@5 {
			reg = <5>;
			label = "cpu";
			ethernet = <&fec1>;
			phy-mode = "rgmii";
			fixed-link {
				speed = <1000>;
				full-duplex;
			};			
        };
	};
					
 };
};

I can read PHY registry by tools like mdio-tool, phytool ect, but i need to modify registry in port. Ethtool can dump port registers by "ethtool -d nmi", but there is no method to write. I need to modify reg 6 (Port-based vlan) to separate ports in switch. How can i do that? In older linux kernels i have /dev/mdio and i can write direct to mdio, in Yocto kirkstone (linux-imx 5.15) i must use ioctl with predefinied structures and commands.

 

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

411件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @MJaroc 

The kernel update could also update the phy driver and mdio framework which will casue older interface can't work. Use ioctl with predefinied structures and commands is also another way to access registers.

 

Best Regards

Zhiming

0 件の賞賛
返信

402件の閲覧回数
MJaroc
Contributor II
Hi @Zhiming_Liu
I sad that there is no predefined structure and command to save registry. I need to add it on my own and modify driver.
0 件の賞賛
返信