Hi all!
I'm trying to build my own Linux that would include all the headers for the Kernel and all the other packages and software installed.
I've included the SDKIMAGE_FEATURES = "dev-pkgs....." in my local.conf
I've run Bitbake with the -c populate_sdk option
I get all the Kernel headers in the image at the usr/include location. But, for example, for "curl" I can't see any headers or separate folder.
Although, in my local yocto/build/tmp/sysroots/..../usr/include, I can find every header for everything installed.
Is there any way to include all the headers that are found on my local build-computer (tmp/sysroots/...) in my image?
Thanks in advance,
Jonas
Hello Jonas
Adding the packages to the SDKIMAGE_FEATURES indeed adds them to the toolchain installer. For adding to your actual image the easiest way would be adding the packages to the IMAGE_INSTALL_append variable so the packages are added to the image. I’m not sure if this would address your problem.
I hope this helps!
Regards,
Hello,
Thanks for your answer.
The packages are all added to my image and the programs works fine. The thing is that I wan't the headers also to be added.
As I wrote earlier, I get all the Kernel headers but not the headers for each "program", for example, curl.
Thanks in advance,
Jonas