Yocto Dunfell GSTREAMER build fails - imx6qdlsabreauto - fsl-framebuffer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Yocto Dunfell GSTREAMER build fails - imx6qdlsabreauto - fsl-framebuffer

607 Views
ycardaillac
Contributor III

Hi,

There's an issue with gstreamer build with imx6qldsabreauto and fsl-framebuffer distro.

I've been reproducing with upstream bsp. Find the repo complete info here : https://pastebin.com/abwRtKAY

meta-freescale : ae2001935fdd7cf7ee7e3b8a4826d7b59202be6d

fsl-community-bsp-base : 5a551f453260bd19895e4d847877874eaa51fde3

meta-freescale-3rdparty : f37f72a85ba273b27347169b727c889f42b91d6c

meta-freescale-distro : 5d882cdf079b3bde0bd9869ce3ca3db411acbf3b

meta-openembedded : 6792ebdd966aa0fb662989529193a0940fbfee00

poky : 90a6f6a110ab14890e2f6a1616e74ee259fc0f8f

Steps to reproduce :

git clone https://github.com/Freescale/fsl-community-bsp-platform.git

cd fsl-community-bsp-platform/

repo init -u https://github.com/Freescale/fsl-community-bsp-platform -b dunfell

repo sync

DISTRO=fsl-framebuffer MACHINE=imx6qdlsabreauto source ./setup-environment build

bitbake fsl-image-machine-test

Relevant part of the failure of gstreamer1.0-plugins-base_1.16.imx :

| Package gstreamer-audio-1.0 was not found in the pkg-config search path.
| Perhaps you should add the directory containing `gstreamer-audio-1.0.pc'
| to the PKG_CONFIG_PATH environment variable
| No package 'gstreamer-audio-1.0' found
| Package gstreamer-video-1.0 was not found in the pkg-config search path.
| Perhaps you should add the directory containing `gstreamer-video-1.0.pc'
| to the PKG_CONFIG_PATH environment variable
| No package 'gstreamer-video-1.0' found

How can I solve this issue?

Best regards,

Yann

0 Kudos
Reply
1 Reply

598 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @ycardaillac 

We provide official support for kirkstone , hardknott ,honister ,gatesgarth ,zeus ,sumo ,thud ,warrior.

Please follow our document to build yocto:

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

Qmiller_0-1665712255915.png

Regards

Zhiming

0 Kudos
Reply