Yocto Codeaurora download is quite slow

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Yocto Codeaurora download is quite slow

1,285件の閲覧回数
petervdperk
NXP Employee
NXP Employee

I've noticed for a couple of weeks now that the download speed of the codeaurora git is quite slow.

I've got a 1000/1000 internet connection but cloning linux-imx is around 200-1500 KiB/s

It really slows down the build time on new machines from couple of hours to almost a full day.

yocto_dl_slow.pngspeed.png

タグ(3)
0 件の賞賛
3 返答(返信)

1,259件の閲覧回数
josephzhou1
Contributor V

speed test to particular server is not the actual speed in the real world .

 

3549 tasks and 5 cores only , build time will be few hours 3-5 hours , it is normal i think . as long as not drops and must rebuild

 

for full image say 6000 build tasks , it is 8--9 hours and / or a day , it is OK what , even here Singapore same same lor

(we even have PREMIRROR server too  still the same speed )

if you got 16 cores , 512 gb memory and 10T hard disk  i guess will be faster , say 15--30 mins done a build ?!

i tesed showed :  multi cores is very important for build , if u use VM please put more cores into Ubuntu than host pc windows.

 

 

Best Regards,
Joseph Zhou Jianhui / Senior Embedded Software Engineer, Singapore
0 件の賞賛

1,263件の閲覧回数
petervdperk
NXP Employee
NXP Employee

Hi @Zhiming_Liu 

I'm not using the VPN and furthermore I've tried it on several other machines and well.
It just seems that the codeaurora mirror for linux-imx is quite slow.

0 件の賞賛

1,271件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @petervdperk 

Do you use VPN of our company?

Not use VPN of our company can also download BSP , and it seems really fast.

 

Regard

Zhiming

0 件の賞賛