Xen port to Colibri IMX8X

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Xen port to Colibri IMX8X

3,300 Views
dwagner
Contributor I

Hello,

I am trying to use the XEN Hypervisor on a Toradex Colibri iMX8X, which features a i.MX8QXP.

My approach is to use the linux-toradex kernel from Toradex BSPs (Details below), made a new Devicetree-File (fsl-imx8qxp-colibri-eval-v3-dom0.dtb) similar to the imx8qm-mek-dom0.dtb and use the same U-Boot Boot-script colibri xenmmcboot - Pastebin.com.

Without Xen the Image boots just fine with the fsl-imx8qxp-colibri-eval-v3-dom0.dtb.

As xen-binary I tried both the imx-xen from your BSPs and the xen-colibri-imx8x from OE/meta-virtualisation and got different resulting errors.

imx-xen

(XEN) *** LOADING DOMAIN 0 ***
(XEN) Missing kernel boot module?
(XEN)
(XEN) ****************************************
(XEN) Panic on CPU 0:
(XEN) Could not set up DOM0 guest OS
(XEN) ****************************************
(XEN)
(XEN) Reboot in five seconds...‍‍‍‍‍‍‍‍‍

complete boot log: xen boot log - Pastebin.com 

xen-colibri-imx8x

[ 0.098234] Xen: initializing cpu0
[ 0.106238] Hierarchical SRCU implementation.
[ 0.119764] Error FSL_HVC_SC -1
[ 0.122594] Cannot request PMIC0_TEMP interrupt
[ 0.127125] Error FSL_HVC_SC -1
[ 0.130206] Cannot request PMIC1_TEMP interrupt
[ 0.134759] Error FSL_HVC_SC -1‍‍‍‍‍‍‍

looks like Xen is running, but at some point "Error FSL_HVC_SC -1" starts appearing. Sadly I couldn't get the (XEN) outputs to show up.

complete boot log: xen-colibri-imx8x boot log - Pastebin.com 

Any suggestions on how to fix/workaround either of both issues?

I would greatly appreciate your inputs!

Setup:

imx-xen

I have build Xen as described in the current https://www.nxp.com/docs/en/user-guide/IMX_YOCTO_PROJECT_USERS_GUIDE.pdf (Rev. L5.4.24_2.1.0, 06/2020)

/imx-yocto-bsp$ MACHINE=imx8qxpmek DISTRO=fsl-imx-wayland source imx-setup-release.sh -b build_imx8/
/imx-yocto-bsp/build_imx8$ bitbake xen‍‍

Dom0

To build Dom0 I use the linux-toradex kernel image provided by toradex OE repo as described here.

Added layer meta-virtualization  = "zeus:1bb515609594215aaf950555211e18c6c9a8e308" to Toradex OE and these to local.conf:

DISTRO_FEATURES_append = " xen virtualization"
IMAGE_INSTALL_append = " xen-base"‍‍
0 Kudos
9 Replies

3,041 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Daniel,

Looks like toradex missing the PMIC or the PMIC is not on the board, the kernel from NXP is for the EVK is not going to work with toradex board.

Regards

0 Kudos

3,041 Views
dwagner
Contributor I

Hello,

thanks for your answer. 
I'm not using NXP's linux-kernel for the EVK, but the one that I built with the Toradex-BSPs, which are based on FSL-/NXP-BSPs. And this kernel is indeed working when booted without the hypervisor. 

Also when booted without hypervisor none of the "Cannot request ___ interrupt" Errors is printed. On top of that I'm sure Toradex has a PMIC on their board, as I have worked with that in the past.

The only thing I am currently using directly from the NXP-BSPs (as described in the Yocto Project Users guide) is the xen binary.

best regards

Daniel

0 Kudos

3,041 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi, Let´s see is someone of toradex‌ can help.

Regards

0 Kudos

3,041 Views
dwagner
Contributor I

Hello,

i was hoping to reach an imx-xen developer or someone that got the Xen part of the i.MX Yocto Project User's Guide running on an board other that the MEK. I can't find any information on what steps are generally nessecary to implement it on an imx-plattform other than in this doc which is specific to the MEK and not much detail is given.

Are the imx-xen developers at nxp(freescale)?

0 Kudos

3,041 Views
Peng_Fan
NXP Employee
NXP Employee

For dom0 dts, did you add something as below?

"

chosen {
#address-cells = <2>;
#size-cells = <2>;

stdout-path = &lpuart0;

/* Could be updated by U-Boot */
module@0 {
bootargs = "earlycon=xen console=hvc0 loglevel=8 root=/dev/mmcblk1p2 rw rootwait";
compatible = "xen,linux-zimage", "xen,multiboot-module";
reg = <0x00000000 0x80a00000 0x00000000 0xf93a00>;
};
};

"

Please also check uboot "run xenmmcboot" or "run xennetboot" to see how it works.

BTW: what usecase would you use xen on 8QX?

Kernel & Virtualization Engineer
0 Kudos

3,041 Views
dwagner
Contributor I

Yes, we have added the following to the dts, which is based on fsl-imx8qxp-mek-dom0.dts - Pastebin.com

chosen {
    #address-cells = <2>;
    #size-cells = <2>;
    module@0 {
          bootargs = "earlycon=xen console=hvc0 loglevel=8 root=/dev/mmcblk0p2 rootwait $
          xen,dom0-bootargs = "console=dtuart dtuart=ttyLP3 earlycon=lpuart32,0x5a090000$
          compatible = "xen,linux-zimage", "xen,multiboot-module";
          /* The size will be override by uboot command */
          reg = <0x00000000 0x80a00000 0x00000000 0xf93a00>;
    };
};
‍‍‍‍‍‍‍‍‍‍‍‍

Additionally to the above, we also adopted all other nodes from mek-dom0.dts to our dts (fsl-imx8qxp-colibri-eval-v3-dom0.dts - Pastebin.com).

I have dissected the xenmmcboot script and to my understanding xenboot_common, which is called by xenmmcboot, also modifies the dtb via fdt set commands.

baudrate=115200
dom0fdt_file=fsl-imx8qxp-colibri-eval-v3-dom0.dtb
fdt_addr=0x83000000
image=Image
loadaddr=0x80280000
mmcdev=0
mmcpart=1
mmcroot=/dev/mmcblk0p2 rootwait rw
xenhyper_bootargs=console=dtuart dtuart=ttyLP3,115200 dom0_mem=2048M dom0_max_vcpus=2 dom0_vcpus_pin=true
xenlinux_addr=0x92000000
xenlinux_console=hvc0 earlycon=xen
 
xenmmcboot=
    setenv get_cmd "fatload mmc ${mmcdev}:${mmcpart}";
    setenv console ${xenlinux_console};
    run mmcargs;
    run xenboot_common;
 
mmcargs=
    setenv bootargs console=${console},${baudrate} root=${mmcroot} video=imxdpufb5:off video=imxdpufb6:off video=imxdpufb7:off
 
xenboot_common=
    ${get_cmd} ${loadaddr} xen;
    ${get_cmd} ${fdt_addr} ${dom0fdt_file};
    ${get_cmd} ${xenlinux_addr} ${image};
    fdt addr ${fdt_addr};
    fdt resize 256;
    fdt set /chosen/module@0 reg <0x00000000 ${xenlinux_addr} 0x00000000 0x${filesize}>;
    fdt set /chosen/module@0 bootargs "${bootargs} ${xenlinux_bootargs}";
    setenv bootargs ${xenhyper_bootargs};
    booti ${loadaddr} - ${fdt_addr};

Our usecase will be to segregate safety critical applications from those that aren't safety critical.

0 Kudos

3,041 Views
jaskis
Contributor II

Hello,

We never did something regarding Xen Supervisor in Toradex. Which Toradex branch did you use to compile the Colibri iMX8X Image.

Best regards, 

Jaski

0 Kudos

3,041 Views
dwagner
Contributor I

Hi,

we are using the 3.0 Version (-b LinuxImage3.0) of your repo to build the linux-kernel

Best regards,

Daniel

0 Kudos

3,041 Views
jaskis
Contributor II

Hi, Thanks for the answer. For Colibri iMX8X PMIC is controlled by the SIU Firmware. Do you have driver/API which make calls from Xen SuperVisor to the SIU Firmware?

Best regards, 

Jaski

0 Kudos