Xen Hypervisor Deployment on SD Card

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Xen Hypervisor Deployment on SD Card

636 次查看
nevozade
Contributor IV

Hello,

I am following the application note AN13138 Xen Deployment on Layerscape Platforms (attached to this issue) to generate Xen hypervisor image and other needed files that work on imx8qm board. I completes the section 2.1 Build by following through the instructions here successfully and I generated the desired files in the desired directory.

However, in the section 2.2 Deployment, there are some tftp commands that should be given on u-boot but because of some problems, I cannot use the tftp properly and I do want to deploy xen hypervisor by using a SD card. Is it possible to load xen_addr, image, device tree blob etc. with SD card and if yes, how?

I would be very grateful if you could help me with running Xen and Dom0.

 

Regards.

标记 (4)
0 项奖励
回复
1 回复

611 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello

 

You may following the yocto user guide document section 5.6.11 to build xen. This is for layerscape not necessarily works for MX8QM.

 

regards

0 项奖励
回复