XBMC ( Kodi ) black-listed gmtime error, workaround?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

XBMC ( Kodi ) black-listed gmtime error, workaround?

989 Views
edwardtyrrell
Senior Contributor I

Hi,

I'd like to use the Krogoth build of XBMC but unfortunately it's blacklisted with an error: "gmtime has not been declared".

Does anyone know how long before this issue will be fixed? Or is there a workaround?

BR,

Ed.

0 Kudos
Reply
3 Replies

801 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Edward Tyrrell,

I would recommend looking at the release information of Kodi and even looking at the Kodi forums for help on building Kodi.

https://github.com/koenkooi/meta-kodi

http://forum.kodi.tv/

You may also look for alternative layers like the one below. Please note that NXP is not responsible for these layers since these are third parties and you may use them at your own risk.

https://github.com/alfonsotames/meta-kodi

Regards,

0 Kudos
Reply

801 Views
edwardtyrrell
Senior Contributor I

Hi,

Thanks, seemed fine until "imx-vpuwrap PROVIDES libfslvpuwrap but was skipped: incompatible with machine imx7dsabresd (not in COMPATIBLE_MACHINE)"

being built with fsl-image-multimedia.

Is this actually the case? Is this version of Kodi not compatible?

BR,

Edward.

0 Kudos
Reply

801 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Edward Tyrrell,

You do not mention which BSP you are using but it is possible that the VPU libraries that are part of the BSP Release may not be compatible. If you are using a BSP Release I would recommend switching to one of the branches of the Community BSP (more information on the link below) since it is part of the Yocto Project and it is Open Source.

http://freescale.github.io/

However, to be sure I would ask on the Kodi forums, although if supported by i.MX machines it’s most likely that it will be based on the Community BSP.

Regards,

0 Kudos
Reply