Hi All,
I am encountering the following issue on both the release of graphics driver (i.e. 3.10.17-1.0.1 and 3.10.17-1.0.1) on i.MX6s based custom board. I have tried 3.10.17-1.0.0 and 3.10.17-1.0.1 version of recipe's for graphics driver and x ddx driver from daisy branch of meta-fsl-arm and also took the binaries of xorg 1.14.4 after building daisy branch using community-bsp to our custom rootfs.
Is this the known issue? Is there any plan to fix this? Could you give some inputs regarding how should I debug and fix if possible?
When I run some x11/gles2.0 example first time after starting the X11 (1.14.4), it works fine, however when I try second time I am seeing following errors. In short X11/GLES2.0 application on exit or killing makes X11 unusable and need to restart the X11 to run the application second time. Is this you also observed?
root@imx6solosabreauto:/opt/
viv_samples/vdk# ./tutorial2_es20 -f 100
systemd[1]: xorg.service: main process exited, code=killed, status=6/ABRT
XIO: fatal IO error 11 (Resource temporarily unavailable) on X server ":0.0"
after 28 requests (28 known processed) with 0 events remaining.
systemd[1]: Unit xorg.service entered failed state.
I also see following in xorg log
[ 49.212] (**) Option "XkbModel" "pc105"
[ 49.213] (**) Option "XkbLayout" "us"
[ 49.349] (II) config/udev: Adding drm device (/dev/dri/card0)
[ 54.636] (EE)
[ 54.636] (EE) Backtrace:
[ 54.636] (EE)
[ 54.637] (EE) Segmentation fault at address 0x65d24000
[ 54.637] (EE)
Fatal server error:
[ 54.638] (EE) Caught signal 11 (Segmentation fault). Server aborting
[ 54.638] (EE)
[ 54.638] (EE)
Regards & thanks,
Vikash
解決済! 解決策の投稿を見る。
Hi Vikash,
I try to reproduce this issue without success, however I tried on Mx6Q, and tutorial2 runs well, So Please try to use the 3.10.17-1.02 version that Includes a graphics driver update with memory, x11 support improvements, deadlock and bug hang fixes
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&fpsp=1&tab=Design_Tools_Tab
If the problem persist please send us the step by step instruction to reproduce the issue on our side with Freescale boards.
Regards
Hi Vikash,
I try to reproduce this issue without success, however I tried on Mx6Q, and tutorial2 runs well, So Please try to use the 3.10.17-1.02 version that Includes a graphics driver update with memory, x11 support improvements, deadlock and bug hang fixes
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&fpsp=1&tab=Design_Tools_Tab
If the problem persist please send us the step by step instruction to reproduce the issue on our side with Freescale boards.
Regards
Thanks for your reply.
It means you can run tutorial2_es02 (or any other application based on x11/gles2.0 api) multiple times on release 3.10.17-1.0.2 however I am using 3.10.17-1.0.0 (only kernel, graphics driver, xddx and xorg). Is it possible to test this on 3.10.17-1.0.0 or 3.10.17-1.0.1 too?
I will try 3.10.17-1.0.2 when it is upstream in daisy or dizzy branch of meta-fsl-arm https://github.com/Freescale/meta-fsl-arm and update.
To reproduce the issue:
- Boot the target
- Start X11
- export DISPLAY=:0.0
- cd /opt/viv_samples/vdk
- ./tutorial2_es02 -f 100 (after this completes run it again)
- ./tutorial2_es02 -f 100 (can't run, seeing the errors I mentioned, to run it again I need to start x11 again)
Regards & Thanks,
Vikash
Now it is working fine. I reinstalled rootfs.
Regards,
Vikash