Hello,
Anyone ported the wl12xx wifi chip driver to imx6 3.10.17 bsp?
Currently we are using 3.0.35 freescale BSP and ported the wifi chip driver successfully. Now we are decided to upgrade the BSP to 3.10.17. Since the 3.10 kernel using the 'device tree concepts', it is very difficult to understand.
Anyone can help me??
Also if any documents are available for adding a new device to board file in 3.10 ?
Regards
Shabeer
已解决! 转到解答。
Hi Ijaz,
Based on boundary devices BSP we ported the wifi modules to our custom board.
Regards
Shabeer
Hi Shabeer,
Have you done the integration?. I am trying to integrate wl1273 wifi module with i.MX. I really appreciate if you could help with the changes in device tree files.
Thank you.
Regards,
Ijaz Fazily
Hi Saurabh,
I am working on kernel version 3.10.17 which has device tree support. But I have doubt that weather the latest release for wl12xx driver supports device tree.
Regards,
Ijaz Fazily
Hi Sinan Akman, sorry for the late replay,i am out of office on last five days..
We are using a custom board based on Sabrelite. The wifi chip is connected to the imx6 through sdio interface( not pcie ).
Do you have any idea to port the wifi driver to 3.10?
Thanks & Regards
Shabeer
Hi Shabeer, I suggest you search for other sdio drivers in the kernel and see how your
hardware differs from them. You could then use those as a base. Also, I would like
to suggest that you port your driver to latest mainline kernel. Not sure if you need to
stay with FSL's 3.10 kernel.
Hope this helps
Sinan Akman