Will 88W8997, 88W8987 be supported on i.MX8MN Win10 IOT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Will 88W8997, 88W8987 be supported on i.MX8MN Win10 IOT

Jump to solution
769 Views
yao_feng
Contributor II

Will NXP plan I.MX Win10 IoT SDK to support 88W8997(WiFi+BT), 88W8987?

customer platform: IMX8M-Nano

 

Check Current versions W21H2-1-5-0, W21H2-1-4-1 only support

88W8897 WiFi+BT

88W8997 WiFi

88W8987 88W8997 

 

 

Ref:

https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/windows-10-iot-ent...

RN:

1.5.0

https://www.nxp.com/docs/en/release-note/IMXWNR.pdf

and 1.4.1

https://www.nxp.com/downloads/en/software-support/WIN10_1.4.1-DOCS.zip

Thanks.

0 Kudos
1 Solution
705 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Correct!.

Regards

View solution in original post

8 Replies
597 Views
sara_sujova
NXP Employee
NXP Employee

Hi @yao_feng @Bio_TICFSL ,

let me correct this answer. There is currently no support for Wifi on Nano, as the board has no PCIe slot. Bluetooth is supported through some general drivers available which enable connecting devices using USB dongle. There are currently no plans scheduled for this feature.


Kind regards,

Sara

0 Kudos
579 Views
yao_feng
Contributor II

Hi @sara_sujova @Bio_TICFSL 
As I know, there is a 88W8987 module on board (AW-CM358) interface: WiFi:SDIO/ BT:UART

Ref:
https://www.nxp.com/design/design-center/development-boards/i-mx-evaluation-and-development-boards/e...)

There is still no plan to support it in next Win10 IOT BSP?

BTW, any other i.mx8 or 9 serious evk will support 88W8987 or 88W8997 (WiFi and BT functions)?

Thanks. 

0 Kudos
560 Views
sara_sujova
NXP Employee
NXP Employee

Hi @yao_feng ,

yes there is a built-in module but those are not supported by Win10IoT, as Win driver source code is not available (Mini, Nano and MQ). 

 There are 2 tested modules:
AW-CM276MA based on 88W8997 (Wifi: PCIe (supported), BT: UART (not supported))
AW-CB178NF  based on 88W8897 (Wifi: PCIe (supported), BT: USB (supported))

There is no plan so far to extend support for different peripheries than PCIe (because of said reasons), or new chips, but i.MX8M, i.MX8M Mini, i.MX8M Plus or i.MX8QXP with WiFi on 88W8997 works with config WiFI: PCIe and BT:USB - since BSP1.4.0. For example module  AW-CM276NF in base configuration should work with both WiFi and BT.

Kind regards,

Sara

 


 

751 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

The 88W8897 and the Mx8MNano is supported in WinIot, Per release note. Maybe I miss something here.

 

Regards

0 Kudos
746 Views
yao_feng
Contributor II

Hi 

Customer is asking 

88W8997 and 88W8987 supported schedule or no schedule

Thanks.

0 Kudos
742 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Correct! is on schedule for next Quarter or next BSP revision.

Regards

0 Kudos
717 Views
yao_feng
Contributor II

Sorry, double confirm in next Win10 IOT BSP revision, both chips will be supported? 

88W8997 WiFi+BT

and 

88W8987 WiFi+BT

 

Thanks.

0 Kudos
706 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Correct!.

Regards