Hi All,
We have ported the driver in Android 7 platform for our wifi device. Driver is installed and while running supplicant we were not able to find the wpa_supplicant related configuration files in /system/etc/wifi/ directory and /data/misc/wifi/ driectory.
Output:
01-01 01:32:26.183 173 423 E WifiHW : VAP created Successfully
01-01 01:32:26.183 173 423 E WifiHW :
01-01 01:32:27.252 173 423 E WifiHW : ****Inside STA wifi.c wifi_get_fw_path out_iface is
01-01 01:32:27.255 427 477 E NetdConnector: NDC Command {22 softap fwreload wlan0 STA} took too long (7071ms)
01-01 01:32:27.255 427 477 E NetworkManagement: wifiFirmwareReload Error reloading wlan0 fw in STA mode: event = 0 22 Ok
01-01 01:32:27.256 427 473 E NetdConnector: NDC Command {23 bandwidth gettetherstats} took too long (1119ms)
01-01 01:32:27.296 173 423 D CommandListener: Setting iface cfg
01-01 01:32:27.296 173 423 D CommandListener: Trying to bring down wlan0
01-01 01:32:27.298 173 423 D CommandListener: Clearing all IP addresses on wlan0
01-01 01:32:27.321 427 477 E WifiMonitor: killSupplicant p2pfalse init.svc.wpa_supplicant=unknown init.svc.p2p_supplicant=unknown
01-01 01:32:27.348 427 477 E wifi : Can not initialize the vendor function pointer table
01-01 01:32:27.348 427 477 E WifiNative-HAL: Could not start hal
01-01 01:32:27.349 427 477 E WifiStateMachine: Failed to start HAL
01-01 01:32:27.349 427 477 E WifiHW : Cannot open "/system/etc/wifi/wpa_supplicant.conf": No such file or directory
01-01 01:32:27.349 427 477 E WifiHW : Wi-Fi will not be enabled
01-01 01:32:27.349 427 477 E WifiStateMachine: Failed to start supplicant!
01-01 01:32:27.361 427 427 E WifiController: WifiControllerWifi turn on failed
01-01 01:32:27.491 1054 1090 D Index : Deleting data for locale 'en_US' took 103 millis
01-01 01:32:27.522 1054 1090 D Index : Indexing locale 'en_US' took 31 millis
Please help me to get supplicant config files in corresponding directory.
Thanks....
Regards,
Raj.
Hi Diego,
Thanks for reply.
Actually the version magic error is cleared by recompiling the driver after modification in kernel imx. So this time we didn't face any issue while inserting the SDIO module.
Could you please give simple explanation for BCMDHD? How dhd module init function is initiating and how SDIO Card is getting registered in SD Host Controller?
Is there any SDIO specification for Android?[like sdio card version..........etc]. Can we use other vendor SDIO card by disabling the BCM in kernel config?
Regards,
Thanaraj.
Hello Thanaraj,
I found this document of how to support a new WiFi card in Android.
Probably, this document can solve your problem.
How to Support New WiFi Card in Android
Best Regards,
Diego.
Hello Raj,
I do not know if you can provide us the driver that the WiFi Module is using, or the name of the driver, that you are using.
Because, we do not have that WiFi Module and unfortunately, I cannot test it by myself. I can only tell you if I can active the driver in the kernel's menuconfig.
Best Regards,
Diego.
Hi Diego,
As you said could please guide us how to active the driver in kernel's menuconfig.
Name of the driver: Redpine Signals Wireless Driver.
You can see the driver in kernel_imx[/drivers/net/wireless/rsi]
Thanks!!!
Regards,
Raj.
For that, you need to go to the following path in the Linux terminal, ~/myandroid/kernel_imx, and type "make menuconfig".
When the kernel configuration menu appears, you need to go to:
Device Drivers --->
Network device support --->
Wireless LAN --->
Press space bar in: Redpine Signal Inc 91x WLAN driver support and save the configuration, without changing the name.
But, you need to build your kernel image separately.
I hope this can solve your problem.
Hi Diego,
As per your suggestion we have enabled our driver in kernel configuration. after this change we try to insert our driver in android platform, but its throwing version magic error,
ERROR:
version magic '4.1.15 SMP preempt mod_unload ARMv7 p2v8 ' should be '4.1.15-dirty SMP preempt mod_unload ARMv7 p2v8 '
And also observed that, if we modify anything in kernel config that time we observed above error. if we use the kernel imx without any change its working fine.
Could you please tell how to make it work by changing kernel config.
Regards,
Thanaraj.
Hello Thanaraj,
In order for a hardware component to properly interface with Android, it must have a corresponding hardware "module" (unrelated to kernel modules) that conforms to the API specified for that type of hardware.
Generally, each type of hardware supported by Android has a corresponding system service HAL definition. There's a Lights Service and a lights HAL definitions. There's a WiFi Service and a WiFi HAL definition.
You need to ask for the Android libraries to RedPine and then retry the kernel configuration with the menuconfig.
Best Regards,
Diego.
Hi Diego,
Yeah. I can understand what you have explained. My question is,
Case 1: Redpine Driver is working properly in android [We have done Wi-Fi & Bluetooth bringup] - without changing kernel part.
Case 2: if i change a single line [just commenting one line ] in kernel, we are getting version magic error. For this we need solution?
For kernel compilation we followed steps in android user guide.
Regards,
Thanaraj.
Hello Raj,
Thank you for writing.
Here it is the left wpa_supplicant.conf. But, it will not work if it is not configured in the kernel. To configure the kernel, you need to set the option in the menu config before you build the Android image.
I hope this can help you.
Best Regards,
Diego.
Hi Diego,
Could you please explain in brief ?.. What option i need to set in Menu config and how to configure Kernel?
As we are not following any separate steps to configure Kernel. Below command only we used to make android image, while making android image itself kernel configuration and compilation done[observed in log],
$ make 2>&1
Thanks!!!
Regards,
Raj.
Hi Diego,
I am using vendor Redpine signals Inc WiFi Module and its driver.
Still we are facing the same issue. Could please tell me the suggestion to fix this issue.
Regards,
Raj.