Why nothing happens after "jumping to os image" in mfg tool?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why nothing happens after "jumping to os image" in mfg tool?

2,029 Views
ahmetkoc
Contributor III


Hello,

I have a imx6 board MCIMX6xAICPU1 board. I downloaded one of the latest mfg tool release from your website. ( L4.1.15_1.1.0_ga-mfg-tools.tar.gz ) I unzipped all the files in same direction. Then did those actions

 

1- connected the Debug UART DB9 to PC.

2-connected USB OTG to PC

3- inserted an empty (also with no partition) SD card to PC. ( We also tried with sd card on board, sd card on both pc and board, no sd card.)

4- Ran the MFG TOOL ( It saw the HID - compliant device)

5 - Press start

6- It loaded uboot, kernel  etc.

7- It reached  the "jumping to os image" state and did nothing else.

 

So SD card  did nothing when we insert it to board. What is the problem?

 

 

 

Original Attachment has been moved to: MfgTool.rar

Labels (1)
Tags (1)
0 Kudos
4 Replies

1,341 Views
aravinthkumarja
Senior Contributor II

Hi ahmetkoc​,

Don't click MFGtool, click your board *.vbs file on same location, Then you can flash it.

If you didn't understand attach entire MFGtool .

Regards,

Aravinth

0 Kudos

1,341 Views
igorpadykov
NXP Employee
NXP Employee

Hi ahmet

please use appropriate *.vbs file (for specific board and boot device), like

mfgtool2-yocto-mx-sabreauto-sdcard-sd3.vbs or other.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos

1,341 Views
ahmetkoc
Contributor III

Hi Igor,

Okay, but how can I do that? I coudn't find such line in ini files or options at anywhere to tell mfg tool to select right .vbs file.

kind regards,

ahmet

0 Kudos

1,341 Views
igorpadykov
NXP Employee
NXP Employee

Hi ahmet

just click with mouse appropriate *.vbs file (for specific board and flashed device),

mfg tools will be launched with necessary for that board and device parameters,

which would be used when ucl2.xml will be executed.

Best regards

igor

0 Kudos